cancel
Showing results for 
Search instead for 
Did you mean: 

Addresses in bootloader are different than tsv?

Mark81
Associate III

During startup I read the following on the console:

INFO:    Loading image id=4 at address 0x2fff0000
INFO:    Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO:    BL2: Loading image id 5
INFO:    Loading image id=5 at address 0xc0100000
INFO:    STM32 Image size : 801160

But those addresses are different than the ones reported into the tsv file:

#Opt	Id	        Name	        Type	IP      Offset	        Binary
-	        0x01	fsbl1-boot	Binary	none	0x0	                tf-a-stm32mp151a-myprj-mx-trusted.stm32
-	        0x03	ssbl-boot	Binary	none	0x0	                u-boot-stm32mp151a-myprj-mx-trusted.stm32
P	        0x04	fsbl1	        Binary	mmc0	0x00004400  tf-a-stm32mp151a-myprj-mx-trusted.stm32
P	        0x05	fsbl2	        Binary	mmc0	0x00044400  tf-a-stm32mp151a-myprj-mx-trusted.stm32

How they are defined?

How to check they are correct?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

TSV file define the address where to program the image within the Flash.

The load address in device memory (SYSRAM, DDR) is different and are defined inside each binary image (likely defined at compile time).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

TSV file define the address where to program the image within the Flash.

The load address in device memory (SYSRAM, DDR) is different and are defined inside each binary image (likely defined at compile time).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here