Skip to main content
iheb
Associate III
September 14, 2022
Solved

How to perform multiple ADC conversions using stm32mp15 ?

  • September 14, 2022
  • 9 replies
  • 3887 views

I am asking this question after using the the Developer package of the STM32 Echosystem in orfer to recompile the kernel drivers of the ADC to activate the ADC, how ever i can't figure out how to modify the device tree. i was trying to get this example "3.3 How to perform multiple ADC conversions in triggered buffer mode using libiio

" provided by st to work (https://wiki.st.com/stm32mpu/wiki/How_to_use_the_IIO_user_space_interface)

how ever when i reach this example to test it doesn't work since i don't have the trigger0 showing up after using the iio_info command

$ iio_readdev -t trigger0 -s 8 -b 8 iio:device0 voltage0 voltage1 | hexdump

in that case my question is how to get this example working by changing the device tree and the developement echosystem's method ?

this is my device tree configuration

&adc {
 vdd-supply = <&vdd>;
 vdda-supply = <&vdda>;
 vref-supply = <&vdda>;
	status = "okay";
 adc1: adc@0 {
 st,min-sample-time-nsecs = <5000>;
 st,adc-channels = <0 1>;
 status = "okay";
 };
 
 adc2: adc@100 {
 status = "okay";
 };
 
 adc_temp: temp {
 status = "okay";
 };
};

This topic has been closed for replies.
Best answer by Erwan SZYMANSKI

Hello @iheb​,

I think you missed the information bubble in chapter 3.1.

Regarding to your configuration that does not work, I think that your timer@6 that is supposed to be used with your failing command is not activated.

Please try to enable it, this is the timer located in stm32mp151.dtsi file:

timers6: timer@40004000 {
	#address-cells = <1>;
	#size-cells = <0>;
	compatible = "st,stm32-timers";
	reg = <0x40004000 0x400>;
	clocks = <&rcc TIM6_K>;
	clock-names = "int";
	dmas = <&dmamux1 69 0x400 0x80000001>;
	dma-names = "up";
	status = "okay";
 
	timer@5 {
		compatible = "st,stm32h7-timer-trigger";
		reg = <5>;
		status = "okay";
	};
};

I modified it directly in the dtsi file to show you, but the clean method is to override the status property in your dts file (More than that, modify it here will not work because the node is overwritten in another DT file). If it is well activated, you will be able to see it in /sys/bus/iio/devices directory. Then, your commands from chaper 3.1 / 3.2 should not fail anymore (except lsiio that is not present on board by default).

Hope it will help to solve your issue.

Kind regards,

Erwan.

9 replies

Erwan SZYMANSKI
ST Technical Moderator
September 14, 2022

Hello @iheb​ ,

In the same article as you mentioned, did you well follow all the chapter 3 (3.1 and 3.2) ?

What is the output of the command lsiio | grep tim ?

In chapter 3.2, did you well assigned the tim6_trgo to your ADC (command echo "tim6_trgo" > trigger/current_trigger)

Please double check these different points and make me a feedback if you still have troubles, and at which step.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
iheb
ihebAuthor
Associate III
September 15, 2022

Hello Erwan,

Thank you for your assistance,

  • Yes, i followed all of chapter 3 (3.1 and 32 as well).

The command

board# lsiio | grep tim

outputs

-sh: lsiio: not found

when i attempt to assign the "tim6_trgo" to the adc i get an error, since i have the same timers when executing iio_info i receive the following output

Library version: 0.15 (git tag: 6ecff5d)
Compiled with backends: local xml ip usb
IIO context created with local backend.
Backend version: 0.15 (git tag: 6ecff5d)
Backend description string: Linux osd32mp1-brk 5.10.10 #1 SMP PREEMPT Sat Jan 23 15:04:06 UTC 2021 armv7l
IIO context has 1 attributes:
 local,kernel: 5.10.10
IIO context has 1 devices:
 iio:device0: 48003000.adc:adc@0 (buffer capable)
 2 channels found:
 voltage0: (input, index: 0, format: le:U16/16>>0)
 3 channel-specific attributes found:
 attr 0: raw value: 886
 attr 1: offset value: 0
 attr 2: scale value: 0.044250488
 voltage1: (input, index: 1, format: le:U16/16>>0)
 3 channel-specific attributes found:
 attr 0: raw value: 795
 attr 1: offset value: 0
 attr 2: scale value: 0.044250488
 2 device-specific attributes found:
 attr 0: trigger_polarity value: rising-edge
 attr 1: trigger_polarity_available value: rising-edge falling-edge both-edges
 2 buffer-specific attributes found:
 attr 0: watermark value: 1
 attr 1: data_available value: 0
 1 debug attributes found:
 debug attr 0: direct_reg_access value: 0x100A

To hear form you soon

Thank you

Iheb

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
September 15, 2022

Hello @iheb​,

I think you missed the information bubble in chapter 3.1.

Regarding to your configuration that does not work, I think that your timer@6 that is supposed to be used with your failing command is not activated.

Please try to enable it, this is the timer located in stm32mp151.dtsi file:

timers6: timer@40004000 {
	#address-cells = <1>;
	#size-cells = <0>;
	compatible = "st,stm32-timers";
	reg = <0x40004000 0x400>;
	clocks = <&rcc TIM6_K>;
	clock-names = "int";
	dmas = <&dmamux1 69 0x400 0x80000001>;
	dma-names = "up";
	status = "okay";
 
	timer@5 {
		compatible = "st,stm32h7-timer-trigger";
		reg = <5>;
		status = "okay";
	};
};

I modified it directly in the dtsi file to show you, but the clean method is to override the status property in your dts file (More than that, modify it here will not work because the node is overwritten in another DT file). If it is well activated, you will be able to see it in /sys/bus/iio/devices directory. Then, your commands from chaper 3.1 / 3.2 should not fail anymore (except lsiio that is not present on board by default).

Hope it will help to solve your issue.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
iheb
ihebAuthor
Associate III
September 15, 2022

hello @Erwan SZYMANSKI​ 

I'm unable to Assign tim7_trgo trigger to ADC, however, I was able to activate the timers and now the iio_info shows the following data.

Library version: 0.15 (git tag: 6ecff5d)
Compiled with backends: local xml ip usb
IIO context created with local backend.
Backend version: 0.15 (git tag: 6ecff5d)
Backend description string: Linux osd32mp1-brk 5.4.31 #7 SMP PREEMPT Thu Sep 15 16:30:06 CEST 2022 armv7l
IIO context has 1 attributes:
 local,kernel: 5.4.31
IIO context has 3 devices:
 iio:device1: 48003000.adc:adc@100 (buffer capable)
 2 channels found:
 voltage0: (input, index: 0, format: le:U16/16>>0)
 3 channel-specific attributes found:
 attr 0: raw value: 1129
 attr 1: offset value: 0
 attr 2: scale value: 0.044250488
 voltage1: (input, index: 1, format: le:U16/16>>0)
 3 channel-specific attributes found:
 attr 0: raw value: 967
 attr 1: offset value: 0
 attr 2: scale value: 0.044250488
 2 device-specific attributes found:
 attr 0: trigger_polarity value: rising-edge
 attr 1: trigger_polarity_available value: rising-edge falling-edge both-edges
 2 buffer-specific attributes found:
 attr 0: watermark value: 1
 attr 1: data_available value: 0
 1 debug attributes found:
 debug attr 0: direct_reg_access value: 0x100A
 iio:device0: 48003000.adc:adc@0 (buffer capable)
 2 channels found:
 voltage0: (input, index: 0, format: le:U16/16>>0)
 3 channel-specific attributes found:
 attr 0: raw value: 227
 attr 1: offset value: 0
 attr 2: scale value: 0.044250488
 voltage1: (input, index: 1, format: le:U16/16>>0)
 3 channel-specific attributes found:
 attr 0: raw value: 434
 attr 1: offset value: 0
 attr 2: scale value: 0.044250488
 2 device-specific attributes found:
 attr 0: trigger_polarity value: rising-edge
 attr 1: trigger_polarity_available value: rising-edge falling-edge both-edges
 2 buffer-specific attributes found:
 attr 0: watermark value: 1
 attr 1: data_available value: 0
 1 debug attributes found:
 debug attr 0: direct_reg_access value: 0x100A
 trigger0: tim7_trgo
 0 channels found:
 3 device-specific attributes found:
 attr 0: sampling_frequency value: 0
 attr 1: master_mode value: reset
 attr 2: master_mode_available value: reset enable update compare_pulse OC1REF OC2REF OC3REF OC4REF

how ever when I execute this command

board# echo "tim7_trgo" > trigger/current_trigger

I receive the following error:

sh: write error: Invalid argument

and if I use for example tim6_trgo as an argument that would yield nothing but when I cat the value of the file it seems to be empty.

therefore I'm still unable to finish the example

the dts file :

...
&timers4 {
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;
	pwm4: pwm {
 pinctrl-names = "default", "sleep";
	 pinctrl-0 = <&pwm4_pins_mx>;
	 pinctrl-1 = <&pwm4_sleep_pins_mx>;
		status = "okay";
	};
};
 
&timers7 {
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;
};
&timers6 {
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;
};
 
&timers8 {
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;
	pwm8: pwm {
 pinctrl-names = "default", "sleep";
	 pinctrl-0 = <&pwm8_pins_mx>;
	 pinctrl-1 = <&pwm8_sleep_pins_mx>;
		status = "okay";
	};
};
...

Thank you

Iheb

Erwan SZYMANSKI
ST Technical Moderator
September 15, 2022

@iheb​ ,

My bad I shared the wrong node, like you said it was timer6 and not timer7.

On which OSTL version are you ? The 4.0 ?

Regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Erwan SZYMANSKI
ST Technical Moderator
September 16, 2022

@iheb​ ,

What I device you is to do the following steps:

In your device tree, add the following part:

/* Test ADC purpose */
&timers5 {
	status = "okay";
};
 
&timers6 {
	status = "okay";
};
 
&adc {
	status = "okay";
};
 
&adc1 {
	status = "okay";
	st,adc-channels = <0 1>;
};

Then, after compilation and deployment, do the following steps on your board shell.

Board$> cd /sys/bus/iio/devices

Board$> ls

You should see something like this in output:

iio:device0 iio:device1 iio:device2 trigger0 trigger1 trigger2 trigger3 trigger4 trigger5 trigger6

Now look at your different device/name to find adc@0 and tim6_trgo:

Board$> cat */name

My output:

40003000.timer:timer@4

48003000.adc:adc@0

48003000.adc:adc@100

tim5_trgo

tim5_ch1

tim5_ch2

tim5_ch3

tim5_ch4

tim6_trgo

tim7_trgo

In my case, I see that adc@0 is iio:device1 and tim6_trgo is trigger5.

Now,

Board$> cd trigger5

Board$> echo 10 > sampling_frequency

Board$> cd ..

Board$> cd iio:device1

Board$> echo 1 > scan_elements/in_voltage0_en

Board$> echo 1 > scan_elements/in_voltage1_en

Board$> echo "tim6_trgo" > trigger/current_trigger

Board$> echo 1 > buffer/enable

Now if I do the multiple ADC conversions command:

Board$> iio_readdev -t trigger5 -s 8 -b 8 iio:device1 voltage0 voltage1 | hexdump

My output:

WARNING: High-speed mode not enabled

0000000 ffff 749e ffff 8660 ffff 8ae9 ffff 8e2c

0000010 ffff 8e30 ffff 8e42 ffff 8eb5 ffff 8f1a

0000020

Can you check these different steps ?

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
iheb
ihebAuthor
Associate III
September 19, 2022

Hello @Erwan SZYMANSKI​ ,

I have followed the exact same steps, it works now i was able to fully follow the tutorial steps by only activating the timers6 on the DTSI file, if I try to activate it on the DTS file it wouldn't work at this point I'm sure it's something to do with me not being able to correctly use the DTS file.

Thank you so much for your help

Iheb

Erwan SZYMANSKI
ST Technical Moderator
September 19, 2022

Hi @iheb​ ,

Glad to see that you solved your issue.

Have a nice day,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.