cancel
Showing results for 
Search instead for 
Did you mean: 

support for FreeRTOS on M33 + Linux on A35 core

TamTran
Associate

Dear All,

I would like to use MYD-LD25X development board, which uses the STM32MP257

 

I plan to run FreeRTOS on the M33 core and Linux on the A35 cores.

Do you know if there are documents that I can follow to run FreeRTOS on M33 core and Linux on the A35 core?

 

 

Thank you very much.

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @TamTran 

Sure this is well supported

Refer to example provided in STM32CubeFWPackage 

See related documentation : 

Category:STM32CubeMP2 Package - stm32mpu

Olivier

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RJL
Associate II

Hi 

I am also doing same thing (FreeRTOS on the M33 core and Linux on the A35 cores) but i dont know how to do this, if you have done this then please guide me how to solve this problem.
also my another aim is to use m33 as master only so if you have any idea about it then please guide me here, i am stuck in this problem since last 30 days and dont know how to do this.