cancel
Showing results for 
Search instead for 
Did you mean: 

M4 ELF build done in CUBEIDE is not uploaded to target on dunfell platform

meiss.M
Associate III

The program can not be uploaded under the dunfell distribution via CUBEIDE 1.3.1 to the target system. Using the thud distribution, target uploads works.

Are there any hidden upload scripts in the CUBEIDE - how to debug the debug upload?

Which yocto packages are necessary to cooperate with the CUBEIDE?

This discussion is locked. Please start a new topic to ask your question.
23 REPLIES 23
OlivierK
ST Employee

Hi,

​The fix is now published.

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v2.0.0

https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note_-_v2.0.0

some cipher methods have been disabled by the community for security reasons.

As a consequence some ssh requests from STM32CubeIDE may not be functional due to the dropbear package configuration.

In this case, you can either:

Best Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
meiss.M
Associate III

Hi Oliver,

thanks for adding this to upstream.

Did you check firmware upload from STMcubeIDE if the the target is missing the directory /lib/firmware.

On my system, firmware upload works, however, a symlink is created:

lrwxrwxrwx   1 root    root           92 Feb 7 17:11 /lib/firmware -> /usr/local/projects/MYPROJECT/lib/firmware/MYPROJEKT_CM4.elf

and IDECube fails with the message: Failed to insert hardware breakpoints: You have requested too many hardware breakpoints/watchpoints.

Can you reproduce this.

OlivierK
ST Employee

​Hi  meiss.M (Community Member)

Indeed, I have the same symlink to the .elf.  But I don't get the message regarding the H/w breakpoint. Could you please share your console log?


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
meiss.M
Associate III

I can share in a couple of days, since the power controller on our dk2 broke yesterday.