2020-08-10 7:53 AM
I'm trying to build linux-5.4.31 for stm32mp1c-ev1 (tag: v5.4-stm32mp-r1). u-boot loads the kernel successfully, but then nothing happens. I've gone in with GDB, and noticed that the kernel is stuck in start_kernel(), and never leaves it.
What is the fix for this?
#0 cpu_v7_do_idle () at arch/arm/mm/proc-v7.S:78
#1 0xc010a1a4 in arch_cpu_idle () at arch/arm/kernel/process.c:71
#2 0xc0158064 in cpuidle_idle_call () at kernel/sched/idle.c:154
#3 do_idle () at kernel/sched/idle.c:263
#4 0xc01583d8 in cpu_startup_entry (state=CPUHP_ONLINE) at kernel/sched/idle.c:355
#5 0xc0acb5b8 in rest_init () at init/main.c:451
#6 0xc0f00a40 in arch_call_rest_init () at init/main.c:573
#7 0xc0f00f10 in start_kernel () at init/main.c:785
#8 0x00000000 in ?? ()
2020-08-12 12:56 AM
Hello @mrnuke ,
I only tried to build the kernel from downloaded file:
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Downloading_the_Linux_kernel
following this instructions (patches, configs, ..)
Could you try the same approach?
In the meantime I'll try rebuild the kernel from github.
Best regards,
Milan
2020-08-12 6:12 AM
Hi @mleo .
I tried with the tarball. I did apply the patches and config fragments. I got identical results.
2020-08-13 6:45 AM
Hi @mrnuke ,
What version ofu-boot do you use? (It might not be compatible).
And just to be sure, could you share with us complete log?
Regards,
Milan
2020-08-13 3:21 PM
Hi @mleo ,
I tried both the u-boot from the meta-st-stm32mp build, and git.denx.de master (commit 99c6953809 ), with the same results.
I noticed that the problem exhibits when using u-boot SPL, but not with TF-A. I went ahead and bisected the stm branch and found the following commit to introduce the issue:
* 21165f3ebcd4 ARM: dts: stm32: move clocks/resets to SCMI resources for stm32mp15This makes no sense to me. Is there a reason it would work with one bootloader, but not the other?
2020-08-13 3:28 PM
I have the exact same problem with the v5.4-stm32mp-r1 github release
I am using vanilla uboot 2020.04
Booting a vanilla kernel works fine, only this one freezes.
Edit: reverting commit 21165f3ebcd4 fixes the problem