2020-07-20 7:53 AM
I'm trying to build the standard st-image-weston image following this guide:
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package
After starting the build with
bitbake st-image-westonWhen it reaches around the 68% of the process I get the following error:
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: oe_runmake failed
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: Execution of '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.21431' failed with exit code 1:
make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
WARNING: exit code 1 from a shell command.
ERROR: Logfile of failure stored in: /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.21431
Log data follows:
| DEBUG: Executing python function tfaconfig_env
| DEBUG: Python function tfaconfig_env finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp157a-dk1.dtb BUILD_PLAT=/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
| ERROR: oe_runmake failed
| make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found. Stop.
| make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.21431' failed with exit code 1:
| make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found. Stop.
| make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile) failed with exit code '1'I haven't added anything besides the cloned repository.
Am I doing something wrong?
Solved! Go to Solution.
2020-07-21 12:33 AM
Please try bitbake -c cleanall tf-a-stm32mp and relaunch.
Hope it help
Olivier
2020-07-20 7:58 AM
Hi @NRosa.1
I notice you are using latest 5.4-Dunfell/V2.0 version.
Some extra package are requested compare to previous 4.19-Thud / V1.2 on Host side.
Please check carefully this section :
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Install_extra_packages
Olivier
2020-07-20 8:11 AM
Hi @Community member ,
I rechecked all of the additional software required and it appears to me that everything is already installed.
Could anything else be the cause of the error?
2020-07-20 8:31 AM
Hi,
>> make: *** No targets specified and no makefile found. Stop.
This is strange.
What is your configuration ( machine, distro ) ?
Thx
Olivier
2020-07-20 8:36 AM
I'm using the standard configuration, that means DISTRO=openstlinux-weston MACHINE=stm32mp1.
As for the OS for the compilation I'm using a Ubuntu 18.04.3 virtual machine using VirtualBox on a Windows 10 enviroment.
2020-07-20 9:01 AM
Hi @NRosa.1
you are working in a fully validated configuration/environment at our end.
Did you have a look to the mentionned log :
Logfile of failure stored in: /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.21431
Does it contain useful info ?
Are you sure the error at do_compile is the first one ? do_fetch succeed ?
Can you make a try of :
bitbake tf-a-stm32mp
Thanks
Olivier
2020-07-21 12:08 AM
Good morning @Community member ,
The content of the log file is basically the same as the error message in the console, and it is the following
DEBUG: Executing python function tfaconfig_env
DEBUG: Python function tfaconfig_env finished
DEBUG: Executing shell function do_compile
NOTE: make -j 4 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp157a-dk1.dtb BUILD_PLAT=/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
ERROR: oe_runmake failed
WARNING: exit code 1 from a shell command.
ERROR: Execution of '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.2316' failed with exit code 1:
make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
WARNING: exit code 1 from a shell command.So unfortunately not very useful.
I suppose that do_fetch had succeeded, but right now it skips directly to do_compile so I'm not sure how can I verify that.
As you can imagine, trying to run bitbake tf-a-stm32mp results in the same exact error in the do_compile.
By the way thanks for all the help and the quick responses.
Noah
2020-07-21 12:19 AM
Hi @NRosa.1
>> I suppose that do_fetch had succeeded, but right now it skips directly to do_compile so I'm not sure how can I verify that.
You should find tf-a sources in "/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source"
Olivier
2020-07-21 12:33 AM
Please try bitbake -c cleanall tf-a-stm32mp and relaunch.
Hope it help
Olivier
2020-07-21 12:40 AM
The folder is empty so it seems to have failed?
Is it possible that do_fetch and do_compile execute in the wrong order?