2023-04-06 9:07 AM
Hello,
We are using st-image-core from recipes-st in yocto and I'm removing some packages from the build that we don't really need. While going through the list, I have found that apt and dpkg are being built and I would like to remove them from my image.
I have tried using SKIP_RECIPE[apt] and SKIP_RECIPE[dpkg] in the local.conf file, but all I get is an error saying they are dependencies:
ERROR: Required build target 'st-image-core' has no buildable providers.
Missing or unbuildable dependency chain was: ['st-image-core', 'apt']ERROR: Required build target 'st-image-core' has no buildable providers.
Missing or unbuildable dependency chain was: ['st-image-core', 'dpkg']I have been digging through the recipes and I couldn't find the dependency for those two packages. Is there any way to remove them from the image?
Thank you.
2023-05-09 4:27 AM
Hi @Jesús Jiménez Sánchez ,
Sorry your post didn't get an answer earlier.
I have no straightforward answer but let me know if you succeed to manage or still stuck.
In that case I would analyze this further.
Olivier
2024-11-17 11:33 PM
If you have the method, please shared it to us.