cancel
Showing results for 
Search instead for 
Did you mean: 

How to check, and eventually enforce Performance governor on STM32MP15 openst-linux?

A.M.
Associate III

I am trying to achieve hard real-time under 100us on the STM32MP157f-eval, specifically, on the Cortex A7 dual core.

Note: I specifically target the Cortex A7 cores because the M4 is already taken for other tasks which requires much smaller latency.

What I did so far is:

  • Build the Yocto openst-linux
  • Add Preempt-RT patch
  • Added several software: irqbalance, tuna, hiccups... to monitor and tune the system.
  • Isolate one core
  • Tested high-priority process, also IRQ. Tested with internal clock and external oscilloscope.
  • Tried to disable most drivers

After all those efforts, the jitter did not improved, and I still get >1ms jitter when applying load for enough time.

------------------------------

My next step is to ensure that the cpu frequency is not throttled.

I read https://wiki.st.com/stm32mpu/wiki/How_to_change_the_CPU_frequency but it's not yet clear to me how to check and set this.

Also, most general questions found on internet don't seem to apply to this architecture.

How to check that cpu frequency is at maximum performance and not throttled?

----------------------------

When using the following command:

$ perf stat -a -A --timeout 10000
 
CPU0                 10003.99 msec cpu-clock                 #    1.000 CPUs utilized
CPU1                 10003.97 msec cpu-clock                 #    1.000 CPUs utilized
CPU0                    184937      context-switches          #   18.486 K/sec
CPU1                     8410      context-switches          #  840.666 /sec
CPU0                        1      cpu-migrations            #    0.100 /sec
CPU1                        1      cpu-migrations            #    0.100 /sec
CPU0                        0      page-faults               #    0.000 /sec
CPU1                        0      page-faults               #    0.000 /sec
CPU0               6498043474      cycles                    #    0.650 GHz
CPU1                176739089      cycles                    #    0.018 GHz
CPU0               2838852339      instructions              #    0.44  insn per cycle
CPU1                 52273406      instructions              #    0.30  insn per cycle
CPU0                471022215      branches                  #   47.083 M/sec
CPU1                  5995202      branches                  #  599.282 K/sec
CPU0                108715456      branch-misses             #   23.08% of all branches
CPU1                  1995755      branch-misses             #   33.29% of all branches

The cycles don't match the maximum, I deduce that the frequency is throttled down.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

@A.M.​ ,

Do you have a netdata service that is running on your target ? It can be easily used to check the CPU frequency over the time. (link here: https://wiki.st.com/stm32mpu/wiki/Netdata)

Rgs,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Erwan SZYMANSKI
ST Employee

Hi @A.M.​ ,

I see that you tried to apply PREEMP-RT patches on our Linux Kernel. Did you take the patches directly from the community or did you use our X-LINUX-RT expansion package ?

If not, please look at this article that can provide you some hints: https://wiki.st.com/stm32mpu/wiki/X-LINUX-RT_OpenSTLinux_Expansion_Package

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Hi @A.M.​ 

To check and affect governor, you either keep only fastest OPP in the device tree or you could try to change it at run time:

cat /sys/devices/system/cpu/cpufreq/policy0/scaling_governor
cat /sys/devices/system/cpu/cpufreq/policy0/scaling_cur_freq
cat /sys/kernel/debug/regulator/regulator_summary | sed -n -e "1p;2p;/vddcore/p"
 
cat /sys/devices/system/cpu/cpufreq/policy0/scaling_available_frequencies
cat /sys/devices/system/cpu/cpufreq/policy0/scaling_available_governors
 
echo performance > /sys/devices/system/cpu/cpufreq/policy0/scaling_governor
 
cat /sys/devices/system/cpu/cpufreq/policy0/scaling_governor
cat /sys/devices/system/cpu/cpufreq/policy0/scaling_cur_freq
cat /sys/kernel/debug/regulator/regulator_summary | sed -n -e "1p;2p;/vddcore/p"

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
A.M.
Associate III

Thank you for your replies.

1) Which PREEMPT-RT patch did I use?: I took the yocto layer from https://github.com/PRG-MPU-ALPHA/meta-st-x-linux-rt. (Witch is the same repo than https://github.com/STMicroelectronics/meta-st-x-linux-rt, before it was made public).

2) @PatrickF​ cat /sys/devices/system/cpu/cpufreq does not exists. I think this is one of the changes made by the PREEMPT_RT layer, according to the answer from Ewan SZYMANSKI.

From those two points, I deduce that the frequency scaling is disabled and always at maximum frequency. Is there a way to check this?

Because from the `perf` results, it look like the CPU frequency is adjusted, which could be a reason for my jitter. It might also be that `perf` tool is not counting `nop` when the core is idle.

@A.M.​ ,

Do you have a netdata service that is running on your target ? It can be easily used to check the CPU frequency over the time. (link here: https://wiki.st.com/stm32mpu/wiki/Netdata)

Rgs,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Erwan SZYMANSKI​ 

Netdata is running, and it was a great discovery to troubleshoot performance.

I could not find any "CPU frequency" there, the cpu usage (<10%) suggest it is at maximum performance, not sure if I missed something.

Regards,

A. Maire

Hi @A.M.​ ,

In the netdata webpage, under "CPU" category, you should see cpufreq graphic.

It shows you the period of time when the CPU run at 800MHz or 650MHz in the case of an MP15 rev F.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hmm, seems not.

Doesn't matter. Thank you.