bitbake st-image-weston cannot connect to bitbake server
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-14 10:43 AM
Hello,
I'm trying to create the Distribution package for my STM32MP157D-DK1.
When I first installed and ran, it said it was running, It stayed that way for the afternoon. I let it 'run' overnight to the same line. I ^C'd out of it. Since then I get this (I just gave the last try)
NOTE: Retrying server connection (#7)... (Traceback (most recent call last):
File "/mnt/c/projects/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/openembedded-core/bitbake/lib/bb/main.py", line 438, in setup_bitbake
server = bb.server.process.BitBakeServer(lock, sockname, configuration, featureset)
File "/mnt/c/projects/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/openembedded-core/bitbake/lib/bb/server/process.py", line 407, in __init__
self.sock.bind(os.path.basename(sockname))
OSError: [Errno 95] Operation not supported
)
WARNING: /mnt/c/projects/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/layers/openembedded-core/bitbake/lib/bb/main.py:469: ResourceWarning: unclosed <socket.socket fd=12, family=AddressFamily.AF_UNIX, type=SocketKind.SOCK_STREAM, proto=0>
logger.info("Retrying server connection (#%d)... (%s)" % (tryno, traceback.format_exc()))
NOTE: Reconnecting to bitbake server...
NOTE: Previous bitbake instance shutting down?, waiting to retry...
NOTE: Retrying server connection (#8)...
ERROR: Unable to connect to bitbake server, or start one (server startup failures would be in bitbake-cookerdaemon.log).
I have deleted Distribution-Package and reloaded to the same end.
I am running ubuntu WSL on Windows 10.
Thanks in advance,
George Roessner
- Labels:
-
STM32MP15 Lines
-
Yocto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-16 11:55 PM
Hi @GeorgeR​ ,
As you may read here https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#WSL2_-28experimental-29
WSL support is only experimental for our distribution.
Please confirm you are using WSL2.
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-18 5:08 AM
Hi Olivier,
Thanks for the answer. Yes, I am using WSL2.
It seems that Linux is needed though. Can this all be done in Windows 10 environment?
Regards,
George
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-19 1:49 AM
Hi @Guenther Roider​ ,
Ok this issue can happen and seems decoralated from WLS2.
To solve it our expert usually remove build folder (build-***) and check no-more process 'bitbake' are running then retry.
Hope it help,
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.