2019-09-24 10:31 AM
I am evaluating different dual-core ARM Cortex-A7 MPUs for their graphical features; one of my requirements is that I need to support a 1280x1024 TFT LCD at 50-60fps using 16 or 24-bit parallel RGB interface.
The evaluation kits offer small LCDs below my requirements, and I need to make sure that the MPUs can support what I need.
Looking at the datasheet for STM32MP157C MPUs, it is clearly stated in multiple places that the upper pixel resolution limit for the LTDC module is WXGA (1366x768) at 60fps. However:
With these assumptions, what ends up being the bottleneck here? Why the oddly-specific WXGA specification in the datasheet?
Thanks!
Solved! Go to Solution.
2019-12-13 7:29 AM
Hi PatrickF, Sorry for the intrusion. I asked this in a separate thread (with now reply, so far :downcast_face_with_sweat: ), How to enable a third party 3.5" NewHaven Display (320x240!!) connected to the LTDC port on STM32MP157C-EV1 board? Do I need to modify some config file to load the LTDC driver, or the device tree files (and rebuild linux...)? I want to display the default apps that come with the STM32MP157C-EV1 on this second 3.5" display. How do I enable the LTCD display driver? Do I physically remove the original 5.5" display form the DSI port?
I also built the OpenCV for ARM7 and used it to capture a Boson thermal imaging camera connected to the USB port on the EV1 board. It works with the 5.5" DSI display (in parallel with the default camera that comes with the board, or my own Logitech USB web cam). I want to display all of this on the 3.5" display mentioned above. Thank you for your help.
(If you don't help me I am going to get fired! NO, JUST KIDDING, but I do not feel all that smart right now! :face_screaming_in_fear: ).
The 3.5" display, NHD-3.5-320240MF-ASXN#, has a Built-in Driver / No Controller and is a 24 bit Interface.
2019-12-13 10:03 AM