cancel
Showing results for 
Search instead for 
Did you mean: 

Can i connect J-Link to test points TP2,TP3,TP4,TP5,TP8,TP9 and not use the embedded ST-Link/V2 ?

ŁMatu.1
Associate

Can i connect J-Link to test points TP2,TP3,TP4,TP5,TP8,TP9 and not use the embedded ST-Link/V2 ? If yes do it needs special treatment like disabling embedded ST-Link/V2 ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hello,

Yes, you could use these points for an external probe.

Should work without specific embedded ST-Link disable (obviously, to avoid conflicts, you must not start any debugging session on ST-Link), and you could still use UART4 VCP thru ST-Link USB.

Please ensure you have the latest ST-Link FW.

Anyway, In case of trouble, you could totally disable ST-Link (debug and VCP) using SB18, or just disconnect ST-Link SWD wires using SB17, SB19 and SB20.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.