Skip to main content
mƎALLEm
ST Technical Moderator
March 18, 2025

How to enable/disable cores on dual-core STM32H7 using STM32CubeProgrammer

Introduction

For various reasons, developers may need to deactivate booting of a core in the STM32H7 dual-core product. This article shows how to disable the Cortex®-M7 and Cortex®-M4 cores and enable them again.

1. Disabling a core in a dual-core configuration

Disabling a core is needed for debug purposes or to turn the product to a single core product. Dual and single core products have the same die, but some features are disabled in production on single core products. The Cortex®-M4 is one of the disabled features. So, you can turn the CM4 off on STM32H745 MCU to be seen as, for example, a STM32H743 MCU by taking care of some hardware specifications like the power supply configuration: SMPS and LDO.
To do so, STM32CubeProgrammer is a fast and easy solution using option bytes. In the next section, we describe how to use this tool to disable/enable Cortex®-M4 and Coretx-M7.
Note: If both cores are disabled in the option bytes, the Cortex®-M7 boots (see section 4). 

2. Disabling and enabling Cortex®-M7 using STM32CubeProgrammer

2.1 Disabling Cortex®-M7 boot

Connect the board with STLINK and open the STM32CubeProgrammer tool:

  1. Go to the option bytes menu by clicking the [OB] button.
  2. Click on the [User Configuration] menu, the menu expands. 
  3. Find the option [BCM7] and uncheck it to disable the Cortex®-M7 boot.
  4. Apply this change by clicking on the [Apply] button and wait for the operation to complete.

Figure 1. Opening option bytes menu in STM32CubeProgrammerFigure 1. Opening option bytes menu in STM32CubeProgrammer

 

 

Figure 2. Disabling the Cortex®-M7 in option bytesFigure 2. Disabling the Cortex®-M7 in option bytes

 

After applying the change in the option bytes, the connection to the MCU is lost. This is normal behavior, and you see these messages:

Figure 3. STM32CubeProgrammer messages after the operation completionFigure 3. STM32CubeProgrammer messages after the operation completion

 To connect to the device again, you need to change the debug access port (see section 4).

2.2 Enabling Cortex®-M7 boot

To enable the Cortex®-M7 boot again, you need first to select the access port 3 to connect to the MCU port (for more details, see section 4):

  1. Go to the Access port menu
  2. Select “3” to enable the access port 3 as shown in the below figure.
  3. Click the [Connect] button to connect to the MCU.

Figure 4. Selecting access port 3 to connect to CM4Figure 4. Selecting access port 3 to connect to CM4

 

After a successful connection, you can see that the CM7 boot is disabled. Check the [BCM7] option again and click on the [Apply] button.

Figure 5. Reenabling the Cortex®-M7Figure 5. Reenabling the Cortex®-M7

 

Wait until the end of the operation. Do not disconnect or power off the board during this operation. At this stage, the Cortex®-M7 is enabled. You can disconnect and reconnect to check.

3. Disabling and enabling Cortex®-M4 using STM32CubeProgrammer

3.1 Disabling Cortex®-M4 boot

Same manipulation steps described in the section 2.1 for Cortex®-M7 but need to uncheck the option “BCM4”.

Figure 6. Disable of the Cortex®-M4 in option bytesFigure 6. Disable of the Cortex®-M4 in option bytes

 Apply this change by clicking on the [Apply] button and wait for the operation to complete.

3.2 Enabling Cortex®-M4 boot

Same manipulation steps described in the section 2.2, but you need to check the option “BCM4”.

Figure 7. Reenabling the Cortex®-M4Figure 7. Reenabling the Cortex®-M4

Wait until the end of the operation. Do not disconnect or power off the board during this operation. At this stage, the Cortex®-M4 is enabled. You can disconnect and reconnect to check.

4. Disabling both cores

There is no usage for this configuration but if the user disables by mistake both cores, there is a mechanism implemented in the MCU to prevent breaking the chip. If both cores are disabled, the Cortex®-M7 keeps booting. This table is provided in the reference manual RM0399:

CM7_CM4_Gated.png

This figure shows that if CM4 and CM7 boot are disabled in the option byte, the connection keeps going over access port 0:

SofLit_0-1738848718961.png

5. Access port number configuration in STM32CubeProgrammer

To differentiate between the two cores in a connection session, the debugger (for example STM32CubeIDE, see the figures 9 and 10) or the STM32Cubeprogarmmer tool need to know which core is active in the current connection. The access port number is used for this purpose in the DP_SELECT register. For more information, refer to reference manual RM0399 debug port access port select register (DP_SELECT) bit description.

Figure 8. APSEL bitfield description in DP_SELECT registerFigure 8. APSEL bitfield description in DP_SELECT register

  • AP0 is the debug access port for the Cortex®-M7
  • AP3 is the debug access port for the Cortex®-M4.

If you disable Cortex®-M7 in the option bytes and the current access port set is 0 in STM32CubeProgrammer, the connection is lost. The same principle applies to Cortex®-M4. If the current active access port is set to 3 in STM32CubeProgrammer and you disable CM4 boot, the connection is lost.

When reestablishing the connection to the MCU, you need to select the access port number corresponding to an enabled core.

Figure 9. Debugger access port configuration of a Cortex®-M7 project in a STM32H7 dual core exampleFigure 9. Debugger access port configuration of a Cortex®-M7 project in a STM32H7 dual core example

 

Figure 10. Debugger access port configuration of a Cortex®-M4 project in a STM32H7 dual core exampleFigure 10. Debugger access port configuration of a Cortex®-M4 project in a STM32H7 dual core example

Conclusion

This article showed how to enable and disable the Cortex®-M7 and Cortex®-M4 boot using STM32CubeProgrammer. 

Related links 

Reference manual 0399: STM32H745/755 and STM32H747/757 advanced Arm®-based 32-bit MCUs.

 

4 replies

Anthony Verbeck
Associate
March 24, 2025

Is there a way to disable the M4 core in STM32CubeIDE? This will disable the core. However, if you are using STM32CubeIDE, it will not know this and inject code into the running core (M7 in this case) to wait for the halted core to synchronize. If STM32CubeIDE was told that the M4 core (in this case) was disabled, it would not generate code for the M4 core and would not inject synchronization code into the M7 core.

mƎALLEm
mƎALLEmAuthor
ST Technical Moderator
March 24, 2025

This article covers the disable/enable of the cores with STM32CubeProgrammer.

"Disable a core with STM32CubeIDE" doesn't make sense as the activation/deactivation is done through the option bytes i.e. in the application.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Anthony Verbeck
Associate
March 25, 2025

OK, so check out this scenario:

I'm working with an STM32H745i-DISCO. I want to use the M7 exclusively.

I follow the outline above and disable the M4 core in STM32CubeProgrammer.

Next, I go into STM32CubeIDE and generate a project for the STM32H745i-DISCO, build it and run it. It will run until it executes the core synchronization code. Then it will freeze because the M4 is disabled (as you've noted by the option bytes) and cannot synchronize with the M7 core.

What I am suggesting is that there should be a way to build a project in STM32CubeIDE so that takes into account the disabled M4 core.

In short, if one core is disabled and you don't modify the code from STM32CubeIDE, then the project will not run. You cannot do one without the other.

 

mƎALLEm
mƎALLEmAuthor
ST Technical Moderator
March 25, 2025

@Anthony Verbeck 

"In short, if one core is disabled and you don't modify the code from STM32CubeIDE, then the project will not run. You cannot do one without the other"

I do agree.

But this is something related to the user code. I mean, that synchronization could be removed by the user and the CubeMx will not generate that code again. The synchronization code is available between 

/* USER CODE BEGIN Boot_Mode_Sequence_X */ and /* USER CODE END Boot_Mode_Sequence_X */

So the user needs to remove the synchronization and program the enabled core.

Keeping one core and disabling the other one is not a regular application scenario for a Dual core product. I don't think a user will purchase a Dual core product than he will use it as a single core (unless per obligation for a reason or another). Disabling a core with STM32CubeProgrammer is used, for example, for debug/tests purposes .

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.