2022-08-30 6:15 AM
There are some parts of the schematic and board view. I was created my own test project from video on YouTube from st.com. Also was tested stm32wb15 example projects with heart rate monitor which are worked.
UPD: APPE_SysUserEvtRx is called
IPCC_C1_TX_IRQHandler is called
IPCC_C1_RX_IRQHandler is called
Also, my option bytes on screenshot
WIRELESS_FW_RUNNING іn stock
SHCI_C2_BLE_Init cause Error Handler with 0x01 code
Solved! Go to Solution.
2022-09-01 12:51 AM
UPD2: Solved.
Set correct option bytes for BOOT.
After CFG_HW_RESET_BY_FW set Disabled
2022-09-01 12:51 AM
2022-12-14 1:19 AM
As I correct in saying you flashed the WB15 example on the WB10 and it worked?
2022-12-14 1:20 AM
I just created my own custom WB10 board but unfortunately there are not any examples to test so curious if this works and if you had to change anything?
2022-12-16 4:41 AM
Oh. Same with me) Trying to create own device with this BLE is mind-blowing. Sure it works if you flashed wb15 example.
2022-12-16 4:45 AM
@Community member I have managed to get the custom template working from scratch on the WB10, basic mycharwrite and mycharnotify so far! but it's progress!
2022-12-16 4:48 AM
@Shahin sure, i thinks same, but now i dealing with error 133 and some magic... :sad_but_relieved_face:
2022-12-16 4:49 AM
I also recommend these videos
https://www.youtube.com/watch?v=YLgEBp7Ibu0&list=PLnMKNibPkDnGbiUxaLBqTdM2nNIVAk_MO
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.