cancel
Showing results for 
Search instead for 
Did you mean: 

Why no Bluetooth signal and phone cannot connect to STM32WB10

Teo
Associate II

There are some parts of the schematic and board view. I was created my own test project from video on YouTube from st.com. Also was tested stm32wb15 example projects with heart rate monitor which are worked.

UPD: APPE_SysUserEvtRx is called

IPCC_C1_TX_IRQHandler is called

IPCC_C1_RX_IRQHandler is called

Also, my option bytes on screenshot

WIRELESS_FW_RUNNING Ñ–n stock

SHCI_C2_BLE_Init cause Error Handler with 0x01 code

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Teo
Associate II

UPD2: Solved.

Set correct option bytes for BOOT.

After CFG_HW_RESET_BY_FW set Disabled

View solution in original post

7 REPLIES 7
Teo
Associate II

UPD2: Solved.

Set correct option bytes for BOOT.

After CFG_HW_RESET_BY_FW set Disabled

Shahin
Associate II

As I correct in saying you flashed the WB15 example on the WB10 and it worked?

I just created my own custom WB10 board but unfortunately there are not any examples to test so curious if this works and if you had to change anything?

Teo
Associate II

Oh. Same with me) Trying to create own device with this BLE is mind-blowing. Sure it works if you flashed wb15 example.

@Community member​ I have managed to get the custom template working from scratch on the WB10, basic mycharwrite and mycharnotify so far! but it's progress!

Teo
Associate II

@Shahin​ â€‹ sure, i thinks same, but now i dealing with error 133 and some magic... :sad_but_relieved_face:

Teo
Associate II