cancel
Showing results for 
Search instead for 
Did you mean: 

Why does the LoRaWAN_End_Node example project not run when debugging on my STM32WL55JC Nucleo-64 board ?

MRubi.2
Associate II

The example project shown below builds and downloads successfully and halts at main(). The ST-LINK appears to connect and start successfully. It is when I click on run that the ST-LINK server says "Target is not responding, retrying..."

I changed absolutely nothing in the source code or header files. This is happening if I attempt to run and debug immediately after importing the default project.

The ST-LINK debugger works with other projects.

Shown below is the precise example project I am using:

0693W00000JNpsGQAT.png 

This is the debugger view, with the program halted at main(), right before I click run:

0693W00000JNppgQAD.png 

Below is the console output after launching the debugger and halting at main():

STMicroelectronics ST-LINK GDB server. Version 5.9.1

Copyright (c) 2021, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

 

Waiting for debugger connection...

Debugger connected

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.8.0          

   -------------------------------------------------------------------

 

ST-Link Server is running on port : 7184

ST-LINK SN : 0034002F3756501520303658

ST-LINK FW : V3J8M3

Board    : NUCLEO-WL55JC

Voltage   : 3.27V

SWD freq  : 12000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x497

Revision ID : Rev Z

Device name : STM32WLxx

Flash size : 256 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0xc3

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a20912.srec

 File     : ST-LINK_GDB_server_a20912.srec

 Size     : 74112 Bytes

 Address    : 0x08000000 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 36]

Download in Progress:

 

File download complete

Time elapsed during download operation: 00:00:02.278

 

Verifying ...

 

Download verified successfully 

And this is the output immediately after I click run:

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Error! Failed to read target status 

Debugger connection lost.

Shutting down...

Here is my CubeMX configuration. I've tried serial wire, JTAG, and disabled:

0693W00000JNq1DQAT.png 

I know that the M0+ core should be the core that most efficiently processes the LoRaWAN stack, but I've run this project before on the M4 core successfully, but am not sure what has changed since then, as I don't have that project anymore.

What am I missing?

Thank you to anyone that can help. I'd appreciate some guidance from the ST's FE's or Application Engineers, if that is possible.

Edit: Here are my debug configurations as well

0693W00000JNq26QAD.png0693W00000JNq2BQAT.png0693W00000JNq2GQAT.png0693W00000JNq2LQAT.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Luca Mainini
Associate II

Most probably you have to enable DEBUG MODE. Go to sys_conf.h and set DEBUGGER_ENABLED to 1. At this point you should be good to go.

View solution in original post

7 REPLIES 7
Luca Mainini
Associate II

Most probably you have to enable DEBUG MODE. Go to sys_conf.h and set DEBUGGER_ENABLED to 1. At this point you should be good to go.

MRuiz.4
Associate II

I have exactly the same issue

MRubi.2
Associate II

The solution was partly answered by LMain.1 (thank you), and partly in the readme.txt included in the project:

0693W00000JPK60QAH.png

MRuiz.4
Associate II

Thanks! Where can I locate the sys_conf.h?

MRubi.2
Associate II

0693W00000JPKChQAP.png

MRuiz.4
Associate II

Thanks! Solved!

Thanks, had the same issue. But if I want to run the program without the debugger, to save battery, how do I proceed?