2025-12-22 7:15 AM
Hi there,
i am planning to create a "smart light" (on/off) which is compatible with philips hue with a stm32wb55RG (nucleo).
I have digged a bit into the numerous examples for zigbee applications and also tried some of them, basically the on/off examples with two boards. They worked and all is fine.
Now i am about to gather informations what would be the best start of getting this into my Hue Bridge.
Currently my Bride does not see those end devices from the example, so i can not add it there.
Does anyone has some kind of Tip or Setup which you can share which is aiming to work with Hue?
Thank you