cancel
Showing results for 
Search instead for 
Did you mean: 

Using SX1276MB1LAS with STM32F767ZI.

SBour.9
Associate II

"The I-CUBE-LRWAN Expansion Package consists of a set of libraries and application examples for STM32L0, STM32L1 and STM32L4 Series microcontrollers acting as end-devices."

Can i use the libraries comming with this package even if i am using a STM32F767ZI and not a STM32Lx?

Simon

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

You'd have to create an equivalent "shim" layer for the F7, so figure the 10-12 L4 files, to F7 equivalents.

A suggested route is to pivot from L4 NUCLEO-64 to NUCLEO-144, and then pivot from L4 NUCLEO-144 to F767ZI NUCLEO-144, and then to your target hardware.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..