TX_POWER field in advertising data
Hello,
I'm currently working with a STM32WB55 and I am here because I would like to set up the advertising data with the following ad types :
- AD_TYPE_SHORTENED_LOCAL_NAME
- AD_TYPE_128_BIT_SERV_UUID_CMPLT_LIST
But it seems that I have not enough space. According to the doc, when we call the aci_gap_set_discoverable() function, 6 extra bytes are automatically added by the stack to the frame (ad flags, and TX_POWER).
My question : Is there a way to remove the TX_POWER field inside the advertising frame ?
I tried to use the aci_gap_delete_ad_type() function, but I got the following returned error : 0x1F (probably "AD_TYPE not found")
Thank you in advance for your support