Skip to main content
Senior
November 26, 2024
Question

STM32WL55 Using LPUART in STOP2 mode with wake-up & clock-switching (HSI-MSI)

Hi,

in my low-power STM32WL55 application I would like to use the LPUART to receive data (no transmission) while the device is in STOP2 mode. I have two questions about this:

  1. The reference manual states:
    "Before entering low-power mode, make sure that no LPUART transfer is ongoing. Checking the BUSY flag cannot ensure that low-power mode is never entered when data reception is ongoing."

    Then how do I check for an ongoing data transfer? The external device connected to the LPUART sends data "spontaneously" so I can't control when this happens, there might be a byte arriving just when I'm entering STOP2 mode. What happens if a reception is ongoing when the device enters STOP2 mode?
  2. I would like to use the HSI oscillator for LPUART reception in STOP2 mode (automatically turning it on when needed). But I would also like to use MSI after wake-up in order to get better flexibility for the CPU frequency (achieving frequencies > 16 MHz, or achieving lower power consumption) by setting STOPWUCK=0. However, keeping both HSI and MSI running results in higher power consumption.

    Is it possible to switch the LPUARTs clock from HSI to SYSCLK after wake-up from STOP2 (via LPUART1SEL=1), or will this result in dropping incoming bytes? Does this work only when MSI=16 MHz (like HSI)?

Thanks in advance!

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
December 19, 2024

Hello @Erlkoenig 

I suggest you take a look at the configuration of this example and modify the clock after waking up to SysCLK. This should work fine.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ErlkoenigAuthor
Senior
December 19, 2024

Hi @STTwo-32 ,

thank you very much. "modify the clock after waking up to SysCLK" - will this also work when SysCLK is not 16 MHz? I guess I have to change LPUART_PRESC while switching the LPUART input clock, but how do I do this atomically, without interrupting an ongoing transfer?

Thanks!