Skip to main content
apous.1
Associate
July 20, 2022
Question

[STM32WB55RG] Launching a default BLE application from latest 1.14.0 Cube release with the stm32wb5x_BLE_Stack_full_extended_fw co-processor firmware?

  • July 20, 2022
  • 2 replies
  • 1189 views

Hi,

I have been trying to launch on a Nucleo WB55 board some default apps available in STM32CubeWB-1.14.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE with the latest version of the BLE_stack_full_extended. (e.g. BLE_HealthThermometer, BLE_Ota)

But then the BLE seems to crash at startup and doesn't even advertise.

If I just replace the co-proc image with the "_full" one instead of "_full_extended", then the example app is working fine.

Any explanation on such a limitation?

Thank you,

Best regards.

This topic has been closed for replies.

2 replies

Remy ISSALYS
ST Technical Moderator
July 21, 2022

Hello,

In order to use the BLE Full stack extended, it is necessary to adapt the scatter file in the BLE applications.

If you want to use extended feature, two examples are available in STM32CubeWB package: BLE_p2pServer_Ext and BLE_p2pClient_Ext.

A wiki page about Wireless Stack will be available soon.

Best Regards

Explorer
July 14, 2023

Hi, I had the same problem. Just replace linker file STM32WB55RGVX_FLASH.ld from the BLE_p2pServer_Ext example. Don't forget to clean your project before.