STM32WB55CE is it possible to compile ZigBee example with other tool than IAR?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-01-31 2:53 AM
Hello,
I tried to build project over KEIL but there is of course problem with linking stm32wb_zigbee_wb_lib.a, keil library has extension ".lib".
Next step i used Atollic and option to import IAR project - compilation failed. Compiler can't find files that should be seen...
So, I tried to build project from beggining. Everything compiling great but there is a problem with linking stm32wb_zigbee_wb_lib.a, some functions are not seen...
Library ".a" for IAR has the same structure that for atollic-gcc? That should work?
- Labels:
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-07 7:02 AM
I've been getting this working over the past few days in TrueStudio, so let me share what it took to get this software compiling:
- I imported the IAR project into TrueStudio
- I replaced the startup file with one generated by TrueStudio. I did this by creating a new project for my processor (in my case STM32WB55RG) and copying the file into my converted project.
- I created a new linker script under File-> New for the same processor.
Then, we need to update the settings for the project in C/C++ Build->Settings:
- Go to the tool settings tab and under C++ Linker->General, select your new linker script .
- Under C++ Linker->Libraries, add stm32wb_zigbee_wb_lib.a under Libraries and add its containing folder to Library Search Path.
At this point, I was able to compile the project. To generate a hex file to program via ST-Link, go to Other->Output Format under the C/C++ Build->Settings Menu, check "Convert Build Output" and select Intel Hex.
Hopefully this helps!