2021-11-01 9:59 PM
2021-11-02 1:06 AM
I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.
Here is the translation of your post using Google translate:
Please inquire if there is a module product with built-in STM32WB.
It would be good if the product passed FCC certification.
If I understand correctly you are looking for a module with the STM32WB.
Yes, it is available and can be found on our website: STM32WB5MMG.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.