NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
We are developing a BLE device based on a STM32WB5MM. The device acts as a server and has configured the connection with bonding (and a passkey).We have a problem connecting to the device when several devices of the same type coexist in the same plac...
I also found programming by serial line in below using STM32F446. Does STM32 has a 'naming convention' for timer, (Like, Basic, Enhanced, etc....), such that I can 'quickly' see if the timer inside our STM32WLE5JC target MCU will have the 'link/slav...
ACI_L2CAP_CONNECTION_UPDATE_RESP_EVENTWhat is the Result field? Need to know if change accepted
Dear All,I am search for an example BLE beacon code for the NUCLEO-WB55RG board which solely uses the HCI layer.There is an example for the WBA board: https://github.com/STMicroelectronics/STM32CubeWBA/tree/main/Projects/NUCLEO-WBA55CG/Applications/B...
I am trying to enable all 3 UARTS (LPUART, USART1 and USART2) within the STM IDE. However, on choosing LPUART, USARTS2 become unavailable (and vice versa) . Is this a device limitation? We really would like to be able to use all 3 uarts (no flow co...
Hi, I would like to disable/re-enable BLE and keep the concurrent Zigbee stack in normal operation. Some other posts suggested to call hci_reset() to disable BLE and re-initialize it later when needed again.After calling hci_reset() somehow Zigbee wo...
Hello all,I have purchased the p-nucleo-lrwan2 set that has a gateway and a end node. In the tools and software they have mentioned how to connect the gateway with LORIOT,TTN and Acitility. But I have a requirement such that gateway and end node-1 (i...
How STM32WLE5JC pin PAD circuit works in mixed 3 volts Vdd and 4.2 volts for Open Drain Output pin? Would like to switch medium power LED that takes 45mA and supplied directly by 4.2 volts Li ion cell. LDO, MCP1700, drops cell voltage from 4.2 to 3V ...
I have found :C:\STM32WL_WS\Hands-on\Point2Point_Phy\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phyand also :C:\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\SubGHz_Phy_PingPongBut it is very difficult to work on this ... by e...
HI,All I noticed that when we use BLE stack, we must set SYSCLK to 16MHz。When i set the SYSCLK upto 100MHz,the uart1 log will be garbled after call BleStack_Init which contained in st ble stack lib。I don't know if my discovery is correct。I don't u...