Router having trouble handling frames
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-07-11 8:03 AM - edited 2023-07-11 8:06 AM
Hello,
I have an OpenThread network with two devices : one end device (STM32WB5MMG) and one router (NUCLEO WB55)
I acquire data with the end device and I try to send 180 000 samples (uint16) to the router
When I try to send, it seems that the router does not handle the data received
Here is the pseudo code sending data for the end device :
typedef struct __attribute__((packed))
{
FrameHeader header;
uint16_t cdf_id;
uint8_t measure_type;
uint16_t sdf_id;
uint16_t total_frame_id;
int8_t data[MAXSDFDATA];
} FrameSDF;
void Acquire(uint8_t ffreq_select, uint32_t samples_to_send) {
//Init
...
//declaration
uint32_t samples_sent = 0;
uint16_t sample_counter = 0;
uint16_t frame_amount = 0;
sampleRes_select = 60000;
samples_to_send = sampleRes_select * 2 * 3;
frame_amount = ceil((float32_t) samples_to_send / (float32_t) MAXSDFDATA);
uint16_t adddressDBG = 0, trial_address = 0;
int16_t acceleration[3];
do {
adddressDBG = Get_I2C_Address(&hi2c1);
trial_address++;
} while (adddressDBG != KX_I2C_ADDRESS && trial_address < 3);
FrameADF adf;
if (adddressDBG == KX_I2C_ADDRESS) {
FrameSDF sdf;
BuildFrame(SDF_SEN, (uint8_t*) &sdf);
sdf.total_frame_id = frame_amount;
HAL_Delay(500);
sdf.sdf_id = 0x0000;
for (int i = 0; i < frame_amount; i++) {
APP_DBG("Frame %d #%d/%d",sdf.sdf_id, i,frame_amount);
APP_DBG("***************************");
int16_t *dataPtr = sdf.data;
if (i == frame_amount - 1) {
sample_counter = samples_to_send - (i * MAXSDFDATA);
} else {
sample_counter = MAXSDFDATA;
}
for (int j = 0; j < sample_counter / 3; j++) { //sample_counter / 3 because 3 values acquired at once
//APP_DBG("Samples #%d", j);
//Acquisitions
...
}
SHCI_C2_RADIO_AllowLowPower(THREAD_IP, FALSE);
APP_THREAD_SDFSend(&sdf, sizeof(FrameSDF));
UTIL_SEQ_WaitEvt(EVENT_ACK_SDF);
HW_TS_Start(timeOutTimerID, (uint32_t) 100);
UTIL_SEQ_WaitEvt(EVENT_TIMER);
sdf.sdf_id++;
samples_sent += sample_counter;
}
sdf.sdf_id = 0x0000; // Reset SDFID because everything was sent.
BuildFrame(ADF_SEN, (uint8_t*) &adf);
adf.error_code = appError;
APP_DBG("****** AppError Value %u ******", adf.error_code);
APP_THREAD_ADFSend(&adf);
UTIL_SEQ_WaitEvt(EVENT_ACK_ADF);
SHCI_C2_RADIO_AllowLowPower(THREAD_IP, TRUE);
UTIL_SEQ_SetEvt(EVENT_SNDCMPLT);
HAL_GPIO_WritePin(VCC_KX_GPIO_Port, VCC_KX_Pin, GPIO_PIN_RESET);
otLinkSetPollPeriod(NULL, 500);
UTIL_LPM_SetStopMode(1 << CFG_LPM_APP, UTIL_LPM_ENABLE);
FeedWDT();
UpdateState(AppState, APP_STATE_SLEEP);
} else {
APP_DBG("Wrong address ERROR");
appError = 0xFF;
BuildFrame(ADF_SEN, (uint8_t*) &adf);
adf.error_code = appError;
APP_THREAD_ADFSend(&adf);
UTIL_SEQ_WaitEvt(EVENT_ACK_ADF);
UpdateState(AppState, APP_STATE_SLEEP);
}
}
Here is the code of the function handling SDF for the router :
static void APP_THREAD_SDFRespHandler(void *pContext, otMessage *pMessage,
const otMessageInfo *pMessageInfo)
{
//TODO Manage SDF response.
APP_DBG("********* SDF Req Handler *********");
uint16_t payloadOffset = otMessageGetOffset(pMessage);
uint16_t payloadLength = otMessageGetLength(pMessage) - payloadOffset;
otMessageRead(pMessage, payloadOffset, PayloadRead, payloadLength);
FrameSDF *sdf=(FrameSDF*)&PayloadRead[0];
APP_DBG("sdf_id %d",sdf->sdf_id);
APP_DBG("sdf_meas %d",sdf->measure_type);
free(sdf);
/* If Message is Confirmable, send response */
if (otCoapMessageGetType(pMessage) == OT_COAP_TYPE_CONFIRMABLE) {
//TODO Send Response
APP_THREAD_CoapSendDataResponse(pMessage, pMessageInfo);
}
}
Here are the logs of both devices (end device on the left / router on the right) :
As you can see, the router is blocked and the end device continues to send data
The error occurring for the end device (err code = 2) is a message drop
I progressively remarked latency for the end device while sending
Do you what could prevent the router to receive data ?
Do you know why the router stays blocked ?
PS : acquisition part and frame allocation was checked and does not seem to be problematic
These two devices are the only devices of the network
- Labels:
-
STM32Cube MCU Packages