cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-WL55J STM32WL Flash Erasing failed after loading the BFU_LoRaWAN_End_Node.bin Please share your inputs to disable the flash write protection.

HVeer.1
Associate II

I have used STM32Cube_FW_WL_V1.1.0 -> LoRaWAN_FUOTA -> 1_Image sample and build the binary file ->  BFU_LoRaWAN_End_Node.bin

After flashing the binary, STM32WL66 Option Bytes got changed and i could not able to erase and update the fflash after that. i tried with mass erase, but it did not help. Please share your inputs to disable the flash write protection.

c:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=swd -ob displ

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.7.0

   -------------------------------------------------------------------

ST-LINK SN : 001600345553500B20393256

ST-LINK FW : V3J7M3

Board    : NUCLEO-WL55JC

Voltage   : 3.26V

SWD freq  : 12000 KHz

Connect mode: Normal

Reset mode : Software reset

Device ID  : 0x497

Revision ID : Rev Z

Device name : STM32WLxx

Flash size : 256 KBytes

Device type : MCU

Device CPU : Cortex-M4

UPLOADING OPTION BYTES DATA ...

 Bank     : 0x00

 Address    : 0x58004020

 Size     : 96 Bytes

██████████████████████████████████████████████████ 100%

 Bank     : 0x01

 Address    : 0x58004080

 Size     : 8 Bytes

██████████████████████████████████████████████████ 100%

OPTION BYTES BANK: 0

  Read Out Protection:

   RDP     : 0xAA (Level 0, no protection)

  BOR Level:

   BOR_LEV   : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)

  User Configuration:

   nBOOT0    : 0x1 (nBOOT0=1)

   nBOOT1    : 0x1 ()

   nSWBOOT0   : 0x1 (BOOT0 taken from PH3/BOOT0 pin)

   SRAM_RST   : 0x1 (SRAM1 and SRAM2 are not erased when a system reset occurs)

   SRAM2_PE   : 0x1 (SRAM2 parity check disable)

   nRST_STOP  : 0x1 (No reset generated when entering the Stop mode)

   nRST_STDBY  : 0x1 (No reset generated when entering the Standby mode)

   nRST_SHDW  : 0x1 (No reset generated when entering the Shutdown mode)

   WWDG_SW   : 0x1 (Software window watchdog)

   IWGD_STDBY  : 0x1 (Independent watchdog counter running in Standby mode)

   IWDG_STOP  : 0x1 (Independent watchdog counter running in Stop mode)

   IWDG_SW   : 0x1 (Software independent watchdog)

   BOOT_LOCK  : 0x1 (CPU1 CM4 Boot lock enabled)

   C2BOOT_LOCK : 0x1 (CPU2 CM0+ Boot lock enabled)

   IPCCDBA   : 0x3FFF (0x3FFF)

  Security Configuration Option bytes ESE:

   ESE     : 0x1 (Security enabled)

  PCROP Protection:

   PCROP1A_STRT : 0xFF (0x803FC00)

   PCROP1A_END : 0x0 (0x8000000)

   PCROP_RDP  : 0x1 (PCROP zone is erased when RDP is decreased)

   PCROP1B_STRT : 0xFF (0x803FC00)

   PCROP1B_END : 0x0 (0x8000000)

  Write Protection:

   WRP1A_STRT  : 0x58 (0x802C000)

   WRP1A_END  : 0x7D (0x803E800)

   WRP1B_STRT  : 0x0 (0x8000000)

   WRP1B_END  : 0xA (0x8005000)

OPTION BYTES BANK: 1

  Security Configuration Option bytes:

   SFSA     : 0x38 (0x38)

   FSD     : 0x0 (System and Flash secure. This bit can only be accessed when HDPADIS = 0)

   DDS     : 0x1 (CPU2 debug access disabled (when also enabled by C2SWDBGEN))

   HDPSA    : 0x7D (0x7D)

   HDPAD    : 0x0 (User Flash hide protection area access enabled.)

   SUBGHSPISD  : 0x1 (FSD=0 and SUBGHSPISD=1: SPI3 security disabled)

   C2OPT    : 0x1 (SBRV will address Flash memory, from start address 0x0800 0000 + SBRV.)

   NBRSD    : 0x1 (SRAM1 is non-secure if FSD=0 and secure otherwise. This bit can only be accessed when HDPADIS = 0)

   SNBRSA    : 0x1F (0x1F)

   BRSD     : 0x0 (SRAM2 is secure if FSD=0 and non-secure otherwise. This bit can only be accessed when HDPADIS = 0)

   SBRSA    : 0x0 (0x0)

   SBRV     : 0xDA00 (0xDA00)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
YBOUV.1
ST Employee

Hi @HVeer.1​ ,

can you please try this?

disable_security.bat

please, let us know

HVeer.1
Associate II

I tried using disabled security.bat, please find herewith the output and share your inputs

0693W00000FCcGBQA1.jpg

YBOUV.1
ST Employee

Hi @HVeer.1​ ,

ESE is active. As long as it is, we can not modify configuration of WRP.

You have to set back to RDP level 1, then regress to RDP level 0 and remove ESE.

Then you will be able to remove WRP protection.

In UM2767 : 8.6 Programming a new software when the securities are activated

best regards