cancel
Showing results for 
Search instead for 
Did you mean: 

How to perform indoor localization AND data transfer pseudo simultaneously

ANist
Associate III

I am new to Bluetooth development so maybe the answer is obvious. I would like to use BLE on a wearable for indoor localization with Eddystone beacons, so far so good. At the same time (or in a timeframe) I would like to transmit information via BLE from the wearable to other devices, does Bluetooth protocol contemplate this feature? Should the localized device switch profile in real-time for localizing, and then for data transmission? Data to be transmitted are integer numbers changing sporadically, I don't need speed but robustness (the integer number must be delivered when a change happens). Thanks!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0