cancel
Showing results for 
Search instead for 
Did you mean: 

Error: --Reserved -- in CubeProgrammer 2.4

Kolab
Senior

Hello! I am trying to download the FUS V1.1.0.0 to a STM32WB5xE controller through SWD in CubeProgrammer so as to update the firmware. But I receive Error: --Reserved-- . I ignored it and downloaded the firmware successfuly but my BLE stack doesn't work :( . I have soldered the controller in my board and connected some peripherals to him and everything is working ех�?еpt BLE. What can I do? Here is the log of CubeProgrammer:

06:13:42 : STM32CubeProgrammer API v2.4.0

06:14:37 : ST-LINK SN : 2A3009013212354D434B4E00

06:14:37 : ST-LINK FW : V2J36S7

06:14:37 : Voltage : 3.19V

06:14:37 : SWD freq : 4000 KHz

06:14:37 : Connect mode: Under Reset

06:14:37 : Reset mode : Software reset

06:14:37 : Device ID : 0x495

06:14:38 : UPLOADING OPTION BYTES DATA ...

06:14:38 : Bank : 0x00

06:14:38 : Address : 0x58004020

06:14:38 : Size : 104 Bytes

06:14:38 : UPLOADING ...

06:14:38 : Size : 1024 Bytes

06:14:38 : Address : 0x8000000

06:14:38 : Read progress:

06:14:38 : Data read successfully

06:14:38 : Time elapsed during the read operation is: 00:00:00.007

06:15:16 : Old Firmware delete ...

06:15:16 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:16 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:16 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:16 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:16 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:16 : Memory Programming ...

06:15:16 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:16 : File : 0x495_FUS_Operator.bin

06:15:16 : Size : 11584 Bytes

06:15:16 : Address : 0x08000000 

06:15:16 : Erasing memory corresponding to segment 0:

06:15:16 : Erasing internal memory sectors [0 2]

06:15:16 : Download in Progress:

06:15:17 : File download complete

06:15:17 : Time elapsed during download operation: 00:00:00.686

06:15:17 : Application is running

06:15:25 : Reconnecting...

06:15:25 : Reconnected !

06:15:26 : Firmware delete Success

06:15:26 : Download Stack/FUS image at address 0x807a000 ...

06:15:26 : Memory Programming ...

06:15:26 : Opening and parsing file: stm32wb5x_FUS_fw.bin

06:15:26 : File : stm32wb5x_FUS_fw.bin

06:15:26 : Size : 24492 Bytes

06:15:26 : Address : 0x0807A000 

06:15:26 : Erasing memory corresponding to segment 0:

06:15:26 : Erasing internal memory sectors [122 127]

06:15:26 : Download in Progress:

06:15:27 : File download complete

06:15:27 : Time elapsed during download operation: 00:00:01.052

06:15:27 : Firmware Upgrade process started ...

06:15:27 : Application is running

06:15:37 : Reconnecting...

06:15:37 : Reconnected !

06:15:37 : Error: -- Reserved --

06:15:37 : Old Firmware delete ...

06:15:37 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:37 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:37 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:37 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:37 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:37 : Memory Programming ...

06:15:37 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:37 : File : 0x495_FUS_Operator.bin

06:15:37 : Size : 11584 Bytes

06:15:37 : Address : 0x08000000 

06:15:37 : Erasing memory corresponding to segment 0:

06:15:38 : Erasing internal memory sectors [0 2]

06:15:38 : failed to erase memory

06:15:38 : failed to erase memory

06:15:38 : Failed to download FUS operator!

06:15:38 : Retry -- 0

06:15:38 : Old Firmware delete ...

06:15:38 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:38 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:38 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:38 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:38 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:38 : Memory Programming ...

06:15:38 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:38 : File : 0x495_FUS_Operator.bin

06:15:38 : Size : 11584 Bytes

06:15:38 : Address : 0x08000000 

06:15:38 : Erasing memory corresponding to segment 0:

06:15:38 : Erasing internal memory sectors [0 2]

06:15:38 : Download in Progress:

06:15:38 : File download complete

06:15:38 : Time elapsed during download operation: 00:00:00.694

06:15:38 : Application is running

06:15:46 : Reconnecting...

06:15:47 : Reconnected !

06:15:48 : Firmware delete Success

06:15:48 : Download Stack/FUS image at address 0x807a000 ...

06:15:48 : Memory Programming ...

06:15:48 : Opening and parsing file: stm32wb5x_FUS_fw.bin

06:15:48 : File : stm32wb5x_FUS_fw.bin

06:15:48 : Size : 24492 Bytes

06:15:48 : Address : 0x0807A000 

06:15:48 : Erasing memory corresponding to segment 0:

06:15:48 : Erasing internal memory sectors [122 127]

06:15:48 : Download in Progress:

06:15:49 : File download complete

06:15:49 : Time elapsed during download operation: 00:00:00.923

06:15:49 : Firmware Upgrade process started ...

06:15:49 : Application is running

06:15:59 : Reconnecting...

06:15:59 : Reconnected !

06:15:59 : Error: -- Reserved --

06:15:59 : Old Firmware delete ...

06:15:59 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:59 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:59 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:59 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:59 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:59 : Memory Programming ...

06:15:59 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:59 : File : 0x495_FUS_Operator.bin

06:15:59 : Size : 11584 Bytes

06:15:59 : Address : 0x08000000 

06:15:59 : Erasing memory corresponding to segment 0:

06:15:59 : Erasing internal memory sectors [0 2]

06:15:59 : failed to erase memory

06:15:59 : failed to erase memory

06:15:59 : Failed to download FUS operator!

06:15:59 : Retry -- 1

06:15:59 : Old Firmware delete ...

06:15:59 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:59 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:59 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:59 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:59 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:59 : Memory Programming ...

06:15:59 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:59 : File : 0x495_FUS_Operator.bin

06:15:59 : Size : 11584 Bytes

06:15:59 : Address : 0x08000000 

06:15:59 : Erasing memory corresponding to segment 0:

06:15:59 : Erasing internal memory sectors [0 2]

06:15:59 : Download in Progress:

06:16:00 : File download complete

06:16:00 : Time elapsed during download operation: 00:00:00.590

06:16:00 : Application is running

06:16:08 : Reconnecting...

06:16:08 : Reconnected !

06:16:09 : Firmware delete Success

06:16:09 : Download Stack/FUS image at address 0x807a000 ...

06:16:09 : Memory Programming ...

06:16:09 : Opening and parsing file: stm32wb5x_FUS_fw.bin

06:16:09 : File : stm32wb5x_FUS_fw.bin

06:16:09 : Size : 24492 Bytes

06:16:09 : Address : 0x0807A000 

06:16:09 : Erasing memory corresponding to segment 0:

06:16:09 : Erasing internal memory sectors [122 127]

06:16:09 : Download in Progress:

06:16:10 : File download complete

06:16:10 : Time elapsed during download operation: 00:00:00.964

06:16:10 : Firmware Upgrade process started ...

06:16:10 : Application is running

06:16:20 : Reconnecting...

06:16:20 : Reconnected !

06:16:20 : Error: -- Reserved --

06:16:20 : Old Firmware delete ...

06:16:20 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:16:20 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:16:20 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:16:20 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:16:20 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:16:20 : Memory Programming ...

06:16:20 : Opening and parsing file: 0x495_FUS_Operator.bin

06:16:20 : File : 0x495_FUS_Operator.bin

06:16:20 : Size : 11584 Bytes

06:16:20 : Address : 0x08000000 

06:16:20 : Erasing memory corresponding to segment 0:

06:16:20 : Erasing internal memory sectors [0 2]

06:16:20 : failed to erase memory

06:16:20 : failed to erase memory

06:16:20 : Failed to download FUS operator!

06:16:20 : Retry -- 2

This discussion is locked. Please start a new topic to ask your question.
25 REPLIES 25
Remi QUINTIN
ST Employee

There is absolutely nothing wrong regarding the values of the option bytes.

So lets go back to basics:

Could you use the batch file I joint to this tread and use it in CLI mode?

Just adapt the paths to you own configuration. (path with ****************)

No need to update the FUS, lets focus on the RF FW.

In the end, there is may be a HW issue with your RF part on this specific custom board.

Kolab
Senior

He complained about  stm32wb5x_BLE_Stack_full_fw.bin (I found it in the batch file "SET RF_STACK_BIN=%BIN_PATH%stm32wb5x_BLE_Stack_full_fw.bin") . But the app was downloaded, and board didn't advertise.

Memory Programming ...

Opening and parsing file: stm32wb5x_BLE_Stack_full_fw.bin

Error: The file stm32wb5x_BLE_Stack_full_fw.bin does not exist, please check the file's path

Error: Failed to download image!

application programming

Remi QUINTIN
ST Employee

just add

echo %FWPATH%

echo %BIN_PATH%

echo %RF_STACK_BIN%

So that the complete path is exposed to determine where the error is in the path.

I expect the error to be in %FWPATH%

Kolab
Senior

The error was in SET RF_STACK_BIN=%RF_STACK_BIN%stm32wb5x_BLE_Stack_full_fw.bin

When I runned the batch , echo %RF_STACK_BIN% returned to me ...\en.stm32cubewb_v1-4-0\STM32Cube_FW_WB_V1.4.0\Projects\STM32WB_Copro_Wireless_Binaries\stm32wb5x_BLE_Stack_fw.bin\STM32Cube_FW_WB_V1.4.0\Projects\STM32WB_Copro_Wireless_Binaries\stm32wb5x_BLE_Stack_fw.bin (a very strange path)

Then I changed like this SET RF_STACK_BIN=...\STM32WB5x\stm32wb5x_BLE_Stack_full_fw.bin then the error disappeared and echo %RF_STACK_BIN% returned a correct path.

But at the end of all the board didn't advertise.

Remi QUINTIN
ST Employee

If you got no error during the programming phase and in the end SFSA is 0x57, then the programming is correct.

The issue should be a HW one on the RF part. Wrong connection to the antenna, adaptive filter not correctly soldered...

Kolab
Senior

thank you very much for the support, i will check the hw.