Can't flash anything on STM32L07
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-07 8:21 PM
Hi,
I'm actually working with a LoRaWAN kit (
https://techship.com/products/acsip-lorawan-evk-antenna-kit-s76sxb/
) based on STM32L073x and Semtech SX1276 radio module.So the kit comes with examples based on Semtech example. I have been able to flash thoses examples via SWD pins and an STM32F0 Discovery ST-Link.But since yesterday, I can't flash anything on the kit. I'm using Keil uVision5. When I try to flash something I get the error message 'No target connected'. I can't even connect with the ST-Link Utility and when I try to set Boot0 High and use STM32 Flash Loader the program crash right after selecting the COM port when I need to select the device in the target list.ST-Link is not the problem as I can still flash on the Discovery board.
I'm really out of idea, I don't know if the MCU is bricked or anything else.
If you have any idea, please tell me beacause I'm totaly stuck at the moment.
Thanks
EDIT : Last time I was able to flash, I tried to change the LoRaWAN region (transmission frequency from ASIA 923 to US 915). I don't remenber if the problem occured right after this change or if I was able to flash one or two more times after that.
#bootloader ##stm32l0 #lorawan- Labels:
-
Bootloader
-
LoRa
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-07 8:41 PM
Can the ST-LINK connect with BOOT0 High?
Is the NRST pin available to the ST-LINK?
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
‎2018-06-07 10:56 PM
Hi
Turvey.Clive.002
and thanks for your consideration.I'm pretty new to STM32 development, specially via SWD pins as I always used discovery boards with embedded ST-Link and this is the first time I use ST-Link for external MCU. Can you explain me how can I check what you are asking me ?
Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-07 11:07 PM
Ok, so you said you tried the Flash Loader when BOOT0 is High, have you tried connecting with the ST-LINK Utilities in that condition? If it connects, erase your code from the device.
The ST-LINK should provide SWCLK, SWDIO, NRST, etc. Do you have all three connected? Can you try selecting the 'Connect Under Reset' mode for the ST-LINK?
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
‎2018-06-07 11:21 PM
Ok I understand now. Yes I tried to set BOOT0 High but ST-Link Utility can't connect to device.
And yes the SWD NRST pin is connected to target RST pin and I selected 'connect under reset' but it does not change anything.
I connected ST-Link to target like this :
GND --> GND
NRST --> RST
SWCLK --> SWC
SWDIO --> SWD
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-18 11:20 PM
So I finnaly succeed to flash something.
First I think there's a problem with the SWD pins, i can't flash anything using the ST-LINK.
I finnaly succed to flash something by seting BOOT0 to high and using the STM32 Flash Demonstrator. I run the program in Windows 7 compatibility and now it works.