Skip to main content
SPuge.1
Associate II
Jul 8, 2021 1:20 PM UTC
Question

BlueNRG-LP and WISE Studio, unable to debug STEVAL-IDB011V1

I try to debug on a STEVAL-IDB011V1 with WISE Studio.

Whatever I try with any project, I have the same error when the debugger tries to launch:

Open On-Chip Debugger 0.11.0+dev-00062-g6405d35f3-dirty (2021-03-26-11:44)

Licensed under GNU GPL v2

For bug reports, read

   http://openocd.org/doc/doxygen/bugs.html

Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.

Info : tcl server disabled

Info : telnet server disabled

Info : CMSIS-DAP: SWD Supported

Info : CMSIS-DAP: FW Version = 0254

Info : CMSIS-DAP: Serial# = 0720000105d6ff333939505043086831a5a5a5a597969908

Info : CMSIS-DAP: Interface Initialised (SWD)

Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1

Info : CMSIS-DAP: Interface ready

Info : clock speed 1200 kHz

Error: Error connecting DP: cannot read IDR

Warn : Flash driver of bluenrg-lp.flash does not support free_driver_priv()

The board is working properly under BlueNRG-LP Navigator and when the binary file build by WISE Studio is programmed with ST BlueNRG Flasher Utility.

What is going wrong with the debug in WISE Studio ?

Do I have to update some software/firmware ?

Thanks

    This topic has been closed for replies.

    5 replies

    MSafr.1
    Associate
    Jul 15, 2021 2:05 PM UTC

    Before debugging hold PUSH1 button, then press RESET button and try to debug your application. Works for me!

    SPuge.1
    SPuge.1Author
    Associate II
    Jul 19, 2021 9:32 AM UTC

    Thanks, it works. I already tried to hold RESET button, but not with PUSH1.

    SPuge.1
    SPuge.1Author
    Associate II
    Jul 29, 2021 2:52 PM UTC

    It works but it take some time - several seconds - to download the software (much more than with older workbench IDE):

    Info : CMSIS-DAP: Interface ready

    Info : clock speed 480 kHz

    Info : SWD DPIDR 0x0bc11477

    Info : bluenrg-lp.cpu: hardware has 4 breakpoints, 2 watchpoints

    Info : starting gdb server for bluenrg-lp.cpu on 3333

    Info : Listening on port 3333 for gdb connections

    Info : accepting 'gdb' connection on tcp/3333

    Warn : GDB connection 1 on target bluenrg-lp.cpu not halted

    undefined debug reason 8 - target needs reset

    target halted due to debug-request, current mode: Thread 

    xPSR: 0xf1000000 pc: 0x10001748 msp: 0x20010000

    target halted due to debug-request, current mode: Thread 

    xPSR: 0xf1000000 pc: 0x10001748 msp: 0x20010000

    Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1507 ms). Workaround: increase "set remotetimeout" in GDB

    Info : Padding image section 0 at 0x1005632c with 4 bytes (bank write end alignment)

    Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1041 ms). Workaround: increase "set remotetimeout" in GDB

    Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1140 ms). Workaround: increase "set remotetimeout" in GDB

    Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1136 ms). Workaround: increase "set remotetimeout" in GDB

    Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1141 ms). Workaround: increase "set remotetimeout" in GDB

    Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1128 ms). Workaround: increase "set remotetimeout" in GDB

    target halted due to debug-request, current mode: Thread 

    xPSR: 0xf1000000 pc: 0x10001748 msp: 0x20010000

    And it works with steps only. As soon as I press resume key, I loose control of the target:

    Error: Error connecting DP: cannot read IDR

    Error: Failed to read memory and, additionally, failed to find out where

    Error: mem2array: Read @ 0x40000004, w=4, cnt=1, failed

    Error executing event resumed on target bluenrg-lp.cpu:

    C:/Ac6/WiSE-Studio/tools/openocd-0.11.0/bin/../share/openocd/scripts/mem_helper.tcl:6: Error: 

    in procedure 'mrw' called at file "C:\Ac6\WiSE-Studio\plugins\fr.ac6.ide.wise.core_1.0.0.202105041516\resources\openocd/series/bluenrg-x.cfg", line 98

    at file "C:/Ac6/WiSE-Studio/tools/openocd-0.11.0/bin/../share/openocd/scripts/mem_helper.tcl", line 6

    Error: Error connecting DP: cannot read IDR

    Do I have to wait for a new release ?

    RGord
    Associate
    May 13, 2022 10:11 AM UTC

    Did you ever solve this problem of being unable to debug if you allow it to run?

    I had the same problem with some of the BLE examples, but not with the peripheral examples.

    For me the problem was caused by the processor going into power saving modes so it was resolved by either by commenting out the call to HAL_PWR_MNGR_Request() or changing POWER_SAVE_LEVEL_STOP_NOTIMER to POWER_SAVE_LEVEL_RUNNING.

    There is probably a more official way of doing this, eg with a Debug build in place of the Release build, but I have not come across one yet.

    Visitor II
    Aug 9, 2024 5:21 PM UTC

    1) Remove/Reinsert the 2 comm USB ports (eval board and debugger) connected to PC

    2) "hold PUSH1 button and press "reset button. Then release PUSH1 button - you can now attach or reflash your device."     as per link      https://community.st.com/t5/stm32-mcus-products/steval-idb011v1-board-cmsis-dap-debugger-failed-to-connect-to/td-p/113325