2025-09-11 12:18 AM - edited 2025-09-11 1:09 AM
I am experiencing an issue with OTA updates on the STM32WB5MMGH6TR when using an Android application. I would like your guidance and support in resolving it.
1. Device / Environment
Device: STM32WB5MMGH6TR
Android app: Custom OTA implementation using BluetoothGatt
ST BLE Sensor Android App versions tested:
ST BLE Sensor 4.18.1 → OTA fails
ST BLE Sensor Classic 4.20.1 → OTA fails
ST BLE Sensor 5.2.10 → OTA works successfully
OTA update fails consistently around 65% when updating to a different firmware version
Updating with the same firmware version works fine.
Android BLE log shows:
- system/stack/gatt/gatt_cl.cc:245 gatt_act_write: gatt_act_write() failed op_code=0x52 rt=143
- system/bta/gatt/bta_gattc_act.cc:1132 bta_gattc_write: write status:0
- system/btif/src/btif_gatt_client.cc:211 btif_gattc_upstreams_evt: Event BTA_GATTC_CONGEST_EVT [24]
Using ST BLE Sensor 5.2.10, OTA completes successfully regardless of firmware version.
Observed behavior:
Chunks sent via WRITE_TYPE_DEFAULT with size ≤ MTU-3
Notifications enabled on for ACKs
0000FE23-8E22-4541-9D4C-21EDAE82ED19Connect to normal mode (A7) → send OTA trigger → disconnect
Connect to OTA mode (A8)
Discover services, request MTU 251, enable notifications
Split firmware into chunks (max 200 bytes, WRITE_TYPE_DEFAULT)
Send next chunk only after STM32 OTA notification ACK
Retry mechanism implemented for failed writes
Observation: Despite proper ACK-driven chunk flow, OTA fails at ~65% when updating to a different firmware version, but works perfectly on THE SAME firmware.
Thansk,
2025-09-29 7:34 AM
Hello @MinhLuu
The OTA should work fine with the ST BLE Sensor, ST BLE ToolBox and the Web Bluetooth (always use the last versions to make sure it works fine).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.