2020-02-02 8:34 AM
Hello,
I develop on both Nucleo-WB55 and my own board with STM32WB55CG.
When I use the Nucleo, everything works fine.
When I use my own baord, I see the device in my smartphone application but I can't connect.
I began to dig in and I found that when I use Nucleo, while connecting to smartphone, the software runs thru state EVT_LE_PHY_UPDATE_COMPLETE.
But when I run on my own board the software doesn't reach to this state.
Why is this different?
I believe I'm using with the same stm32wb5x_BLE_Stack_fw.bin.
Thanks,
Lior Malik
Solved! Go to Solution.
2020-02-05 1:28 AM
I found the problem.
Because I work with internal oscillator for the BLE, the define CFG_BLE_LSE_SOURCE must be set to 1 for internal source.
2020-02-05 1:28 AM
I found the problem.
Because I work with internal oscillator for the BLE, the define CFG_BLE_LSE_SOURCE must be set to 1 for internal source.
2020-02-11 6:40 AM
Perfect!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.