Skip to main content
du00000001
Associate
August 14, 2019
Question

What's the best way to disable the DSI (mainly in terms of EMC) ?

  • August 14, 2019
  • 2 replies
  • 892 views

Hard to believe, we have an F469 MCU (chosen due to a number of attributes) that will not use the DSI.

Other than with standard GPIOs, were unused pins are configured as outputs and set to 0 (zero), this doesn't seem to be possible with the DSI I/O pins. Now what ?

Best regards

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
August 14, 2019

What's the issue?

Can't you just disable, or not configure the interface, and just tied the pins off with pull downs?

Perhaps discuss concerns with the local FAE supporting your account? Contact local sales office.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
du00000001
Associate
August 14, 2019

Tieing the pins down is an option.

Just asking to make sure we didn't miss something comparable to the active "controlled low" of the GPIOs.