cancel
Showing results for 
Search instead for 
Did you mean: 

Unresponsive Buttons on STM32F7 Disco After Holding Click

NB1
Associate II

Hello everyone,

I added two buttons (the button type is shown in the attached picture) to my UI, each controlling two relays with the STM32F7 Disco. When I maintain a click on one of the buttons, both buttons turn off and become unresponsive. I need to reset the board to make them functional again.

Can anyone explain why the UI behaves this way and suggest a solution?

Thanks,

BR,

Nourhene.

NB1_0-1721584212032.png

 

3 REPLIES 3

Hello @NB1 ,

In your code, how do you handle the switching between the buttons? I think it would be way easier to just use the Toggle Button widget in the TouchGFX designer which already implements the behavior you are looking for.

Please give it a try and test if the same issue still exists

Best regards, 

Mohammad MORADI
ST Software Developer | TouchGFX

Hello @Mohammad MORADI ESFAHANIASL,

Thank you for your response. I believe we are discussing the same widget. I am also using the button you mentioned, but the code I generated is slightly different from the code provided in this link: Toggle Button.

My question is: Could this difference be the reason for the issues I'm experiencing with my buttons?

Here is my generated code:

#include <gui_generated/screen1_screen/Screen1ViewBase.hpp> #include <touchgfx/Color.hpp> #include <images/BitmapDatabase.hpp> Screen1ViewBase::Screen1ViewBase() { __background.setPosition(0, 0, 800, 480); __background.setColor(touchgfx::Color::getColorFromRGB(0, 0, 0)); add(__background); toggleButton1.setXY(345, 215); toggleButton1.setBitmaps(touchgfx::Bitmap(BITMAP_ALTERNATE_THEME_IMAGES_WIDGETS_TOGGLEBUTTON_MEDIUM_ROUNDED_ON_NORMAL_ID), touchgfx::Bitmap(BITMAP_ALTERNATE_THEME_IMAGES_WIDGETS_TOGGLEBUTTON_MEDIUM_ROUNDED_OFF_LIGHT_ID)); add(toggleButton1); } Screen1ViewBase::~Screen1ViewBase() { } void Screen1ViewBase::setupScreen() { }

 

I can see that you have assigned to action to your button.
How do you control the communication between the toggle and your relays? 

Mohammad MORADI
ST Software Developer | TouchGFX