cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX project not working on STM32H747I Disco

radescu
Associate II

Hello Everyoane,

I'm new here and I'm trying to set up my first project. I don't have experience with the STM board, so I don't know where the problem starts.

To check the boards, I'm using some templates from TouchGFX Designer and writing on my board. The problem that I have is that is not working correctly at all. I don't have texts or instead of the graphic (one analog clock), for example, I have just a white square. Also, if I load an image and try to display it, it's just a white square on the display ( after I write the program).

If I'm usind text, on the display I have pixel problems.

Can I have some advice, please?

Thank you!

Alex

11 REPLIES 11

Little additional info... you choice most complex board of high level STM without experience, then result is clear...

MM1_0-1744314870038.png

and FYI in designer first step choice board, exist pulldown menu with versions fw variants. Not all works on all board variants. Next point is TGFX version not always latest is best choice usw.

 

radescu
Associate II

Thank you for your post, Mr. MM..1,

I chose that complex board for industrial applications to avoid using a PC and use Visual Studio for programming, mainly because of the dimensions of the board, compared with the PC.

I hope I will manage to make my projects.

Once again, thank you for your involvement and your valuable advice.