cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX designer 4.24.0 cannot create a new project by any samples

Chand446209
Associate II

TouchGFX designer 4.24.0 is new installed in my laptop which is Win11. I used the Clock Example to create a project, and reported an error. The log is attached.

Chand446209_0-1727140779804.png

I also created a new project by simulator. I put a button and run the simulator. It was fail. The log is attached too.

Did I miss something to install?

 

 

11 REPLIES 11

Hi @GaetanGodart ,

 

Thanks for your help.

I compared the log in the post with mine. I think it is not the same error. 

My log showed that it cannot load something from server.

[14] ERROR Utils.WebHandling.WebHandler: One or more errors occurred. (Response status code does not indicate success: 404 (Not Found).)

But the log in the post you mention is cannot load something local.

ERROR TouchGFXDomainModel.LoadSave.LoadSave: C:/TouchGFX/4.22.1/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/win32/registry.rb:910:in `encode': U+0131 to IBM437 in conversion from UTF-16LE to UTF-8 to IBM437 (Encoding::UndefinedConversionError)

I tried this solution in my Win11, but it didn't work.

Hello @Chand446209 ,

 

Have you had any success in fixing that issue?
It is definitely related to your environment so I cannot reproduce the issue which makes it hard to understand for me but if it is related to loading something from server, I would advise to check your proxy (in system and in TouchGFX Designer) and to try to change it and see if anything improves.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)