2024-09-23 06:30 PM
TouchGFX designer 4.24.0 is new installed in my laptop which is Win11. I used the Clock Example to create a project, and reported an error. The log is attached.
I also created a new project by simulator. I put a button and run the simulator. It was fail. The log is attached too.
Did I miss something to install?
2024-09-24 02:54 AM
Hello @Chand446209 and welcome to the community! :smiling_face_with_smiling_eyes:
I checked the logs but did not see anything obvious.
Did you also download STM32CubeIDE and STM32CubeProgrammer?
I advise you to follow this tutorial to properly install TouchGFX : How to TouchGFX: Installing TouchGFX Designer for STM32 GUI applications
I hope this helps!
Regards,
2024-09-30 07:38 AM
Hello @Chand446209 ,
Were you able to move forward on your issue?
Regards,
2024-10-11 06:52 PM
Sorry for late response.
I uninstalled my cubeide and touchgfx and removed all the related folder in C drive. After that, install cubeide 1.16.1, touchgfx designer 4.24.0 and touchgfx generator 4.24.0 in cubeide by following your suggestion.
Finished all the steps, I created a new project in designer, put a button and run simulator. The same errors were shown.
Do you have any idea if there were any step I missed?
Thanks for you help.