2023-07-30 5:06 PM
Hi,
I've installed TouchGFX following the instruction at https://support.touchgfx.com/docs/introduction/installation on a completely new installation of windows 10. When I try to create a project, TouchGFX crashes at 88% and simply closes. When I checked the TouchGFXDesigner.log file the error is System.IO.FileLoadException: Failed to load native freetype library!
Any idea how I can fix this?
Please see attached log file.
Thank for your help. Looking forward to get the designer working.
Richard
Solved! Go to Solution.
2025-06-20 8:06 AM
i had same issue and resolved by updating version of Visual C++ to latest