2020-04-28 3:14 AM
Hello, I and using Touchgfx in my project. I want to implement below.
1) During run time , I want to to turn off complete screen.
2) During run time , I want to change complete screen.
3) I want to generate QR code dynamically and also want to clear it sometimes during run time. I got github link and added those files in my project. Still I am not sure how to call it. You have mentioned to call qrCode.setXY(0,0) , qrCode.setQRCode(&code), qrCode.setScale(4) , add(qrCode) methods but I am unable to find it.
Can any one please help ?
Solved! Go to Solution.
2024-09-04 5:32 AM
Ref Code from above attached file
ScreenView.C
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
add(QRCode);
updateQR("Hello"); //Successfully Generates QR Code for "Hello"
}
//Calling updateQR(char* string,uint8_t size) through modelListener
void Screen1View::updateQR(char* string)
{
QRCode.setScale(4);
QRCode.setQRCodeVersion(5);
QRCode.setErrorCorrectionLevel(qrcodegen_Ecc::qrcodegen_Ecc_LOW);
QRCode.convertStringToQRCode(string);
resizeScreen();
QRCode.setXY(38, 38);
QRCode.invalidate(); //Here I am unable to generate QR Code from string received via UART.
}