2021-04-29 9:27 AM
Hello!
I have problem with initialization MIPI DSI interface on STM32H747. I use this interface for connect round LCD display with the St7797 display controller. But the problem is that when sending a sequence of LP commands to initialize the display, there is no data on the D0P and D0N lines. In this case, the signal is constantly present on the CLK lines.
I am attaching a test project with settings. Tell me where the problem might be?
UPDATE: If use LTDC controller, video data present on data line.
But there is nothing on the data lines when sending init commands to display.
I am attaching a test CubeIDE project with interface initialization.
Regards, Alex
2021-04-29 10:20 AM
Hi @AlexVetoshko ,
Please refer to the STM32CubeH7 LCD_DSI example under the following location: Projects\STM32H747I-DISCO\Examples
Best Regards,
Ons.
2021-05-01 9:29 AM
Hello!
Yes, I looked at this example. In this example, commands are transmitted normally. But there the DSI module is used in a different mode (Adaptive Command Mode). My display requires video mode. And in this mode, I cannot send LP commands for initialization (I do not see any signals on the data line). Because of this, I can not initialize the display controller. In this case, the video data (when the LTDС module is turned on) is normal. What is the problem?
Can you help me?
I am attaching the code with the initialization of the DSI module:
static void MX_DSIHOST_DSI_Init(void)
{
DSI_PLLInitTypeDef PLLInit = {0};
DSI_HOST_TimeoutTypeDef HostTimeouts = {0};
DSI_PHY_TimerTypeDef PhyTimings = {0};
DSI_VidCfgTypeDef VidCfg = {0};
/* USER CODE BEGIN DSIHOST_Init 1 */
/* USER CODE END DSIHOST_Init 1 */
hdsi.Instance = DSI;
hdsi.Init.AutomaticClockLaneControl = DSI_AUTO_CLK_LANE_CTRL_ENABLE;
hdsi.Init.TXEscapeCkdiv = 2;
hdsi.Init.NumberOfLanes = DSI_ONE_DATA_LANE;
PLLInit.PLLNDIV = 10;
PLLInit.PLLIDF = DSI_PLL_IN_DIV1;
PLLInit.PLLODF = DSI_PLL_OUT_DIV1;
if (HAL_DSI_Init(&hdsi, &PLLInit) != HAL_OK)
{
Error_Handler();
}
HostTimeouts.TimeoutCkdiv = 1;
HostTimeouts.HighSpeedTransmissionTimeout = 0;
HostTimeouts.LowPowerReceptionTimeout = 0;
HostTimeouts.HighSpeedReadTimeout = 0;
HostTimeouts.LowPowerReadTimeout = 0;
HostTimeouts.HighSpeedWriteTimeout = 0;
HostTimeouts.HighSpeedWritePrespMode = DSI_HS_PM_DISABLE;
HostTimeouts.LowPowerWriteTimeout = 0;
HostTimeouts.BTATimeout = 0;
if (HAL_DSI_ConfigHostTimeouts(&hdsi, &HostTimeouts) != HAL_OK)
{
Error_Handler();
}
PhyTimings.ClockLaneHS2LPTime = 20;
PhyTimings.ClockLaneLP2HSTime = 18;
PhyTimings.DataLaneHS2LPTime = 10;
PhyTimings.DataLaneLP2HSTime = 13;
PhyTimings.DataLaneMaxReadTime = 0;
PhyTimings.StopWaitTime = 0;
if (HAL_DSI_ConfigPhyTimer(&hdsi, &PhyTimings) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_ConfigFlowControl(&hdsi, DSI_FLOW_CONTROL_BTA) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_SetLowPowerRXFilter(&hdsi, 10000) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_ConfigErrorMonitor(&hdsi, HAL_DSI_ERROR_NONE) != HAL_OK) // HAL_DSI_ERROR_NONE
{
Error_Handler();
}
LPCmd.LPGenShortWriteNoP = DSI_LP_GSW0P_ENABLE;
LPCmd.LPGenShortWriteOneP = DSI_LP_GSW1P_ENABLE;
LPCmd.LPGenShortWriteTwoP = DSI_LP_GSW2P_ENABLE;
LPCmd.LPGenShortReadNoP = DSI_LP_GSR0P_ENABLE;
LPCmd.LPGenShortReadOneP = DSI_LP_GSR1P_ENABLE;
LPCmd.LPGenShortReadTwoP = DSI_LP_GSR2P_ENABLE;
LPCmd.LPGenLongWrite = DSI_LP_GLW_ENABLE;
LPCmd.LPDcsShortWriteNoP = DSI_LP_DSW0P_ENABLE;
LPCmd.LPDcsShortWriteOneP = DSI_LP_DSW1P_ENABLE;
LPCmd.LPDcsShortReadNoP = DSI_LP_DSR0P_ENABLE;
LPCmd.LPDcsLongWrite = DSI_LP_DLW_ENABLE;
LPCmd.LPMaxReadPacket = DSI_LP_MRDP_ENABLE;
LPCmd.AcknowledgeRequest = DSI_ACKNOWLEDGE_ENABLE;
if (HAL_DSI_ConfigCommand(&hdsi, &LPCmd) != HAL_OK)
{
Error_Handler();
}
/*Video Mode initialization*/
VidCfg.VirtualChannelID = 0;
/*DSI Host Color format configuration. The image data is transmitted using Packed Pixel Stream with 24 bit format.*/
VidCfg.ColorCoding = DSI_RGB888;
VidCfg.LooselyPacked = DSI_LOOSELY_PACKED_DISABLE;
/*Video mode configuration*/
VidCfg.Mode = DSI_VID_MODE_BURST;
/*Video packet configuration*/
VidCfg.PacketSize = 400;
VidCfg.NumberOfChunks = 0;
VidCfg.NullPacketSize = 0;
/*Signal polarity configuration. Same polarity between LTDC and DSI except for Data Enable which has opposite polarity */
VidCfg.HSPolarity = DSI_HSYNC_ACTIVE_LOW;//correct
VidCfg.VSPolarity = DSI_VSYNC_ACTIVE_LOW;//correct
VidCfg.DEPolarity = DSI_DATA_ENABLE_ACTIVE_HIGH;//correct
/*Video timing configuration. Retrieved from LTDC config*/
VidCfg.HorizontalSyncActive = HSYNC * LBCLK_PCLK_MULT; //lane byte clock cycles
VidCfg.HorizontalBackPorch = HBP * LBCLK_PCLK_MULT; //lane byte clock cycles
VidCfg.HorizontalLine = (HSYNC + HBP + HACT + HFP) * LBCLK_PCLK_MULT; //lane byte clock cycles
VidCfg.VerticalSyncActive = VSYNC;
VidCfg.VerticalBackPorch = VBP;
VidCfg.VerticalFrontPorch = VFP;
VidCfg.VerticalActive = VACT;
/*Command transmission mode and Max LP packet size*/
VidCfg.LPCommandEnable = DSI_LP_COMMAND_ENABLE;
VidCfg.LPLargestPacketSize = 29;
VidCfg.LPVACTLargestPacketSize = 8;
/*LP transition configuration. It is recommended to enable LP transition in all regions*/
VidCfg.LPHorizontalFrontPorchEnable = DSI_LP_HFP_ENABLE;
VidCfg.LPHorizontalBackPorchEnable = DSI_LP_HBP_ENABLE;
VidCfg.LPVerticalActiveEnable = DSI_LP_VACT_ENABLE;
VidCfg.LPVerticalFrontPorchEnable = DSI_LP_VFP_ENABLE;
VidCfg.LPVerticalBackPorchEnable = DSI_LP_VBP_ENABLE;
VidCfg.LPVerticalSyncActiveEnable = DSI_LP_VSYNC_ENABLE;/*Flow control configuration*/
VidCfg.FrameBTAAcknowledgeEnable = DSI_FBTAA_ENABLE;//needed for commands in video mode
if (HAL_DSI_ConfigVideoMode(&hdsi, &VidCfg) != HAL_OK)
{
Error_Handler();
}
if (HAL_DSI_SetGenericVCID(&hdsi, 0) != HAL_OK)
{
Error_Handler();
}
__HAL_LTDC_DISABLE(&hltdc);
HAL_DSI_Start(&(hdsi));
LOG_INFO("Start display init\r\n");
LCD_Reset();
HAL_Delay(120);
St7797_Init_sequence();
LOG_INFO("Disable command mode \r\n");
LPCmd.LPGenShortWriteNoP = DSI_LP_GSW0P_DISABLE;
LPCmd.LPGenShortWriteOneP = DSI_LP_GSW1P_DISABLE;
LPCmd.LPGenShortWriteTwoP = DSI_LP_GSW2P_DISABLE;
LPCmd.LPGenShortReadNoP = DSI_LP_GSR0P_DISABLE;
LPCmd.LPGenShortReadOneP = DSI_LP_GSR1P_DISABLE;
LPCmd.LPGenShortReadTwoP = DSI_LP_GSR2P_DISABLE;
LPCmd.LPGenLongWrite = DSI_LP_GLW_DISABLE;
LPCmd.LPDcsShortWriteNoP = DSI_LP_DSW0P_DISABLE;
LPCmd.LPDcsShortWriteOneP = DSI_LP_DSW1P_DISABLE;
LPCmd.LPDcsShortReadNoP = DSI_LP_DSR0P_DISABLE;
LPCmd.LPDcsLongWrite = DSI_LP_DLW_DISABLE;
LPCmd.LPMaxReadPacket = DSI_LP_MRDP_DISABLE;
LPCmd.AcknowledgeRequest = DSI_ACKNOWLEDGE_DISABLE;
if (HAL_DSI_ConfigCommand(&hdsi, &LPCmd) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DSIHOST_Init 2 */
/* USER CODE END DSIHOST_Init 2 */
}
2021-05-26 8:12 AM
Hi Ons KOOLI (ST Employee)
Can you help us?
We really need to know, it's very critical on this moment for us.
2021-05-27 1:02 AM
Hi @wrfrf.1 ,
I am rising your claim internally to get help from specific dev team.
Best Regards,
Ons.
2021-05-28 5:22 AM
Hi @wrfrf.1 ,
As recommended by our dev team, can you disable the AutomaticClockLaneControl:
hdsi.Init.AutomaticClockLaneControl = DSI_AUTO_CLK_LANE_CTRL_DISABLE;
and inform me if this fixes the problem.
Best Regards,
Ons.
2021-05-28 7:33 AM
Hi Ons KOOLI ! We have checked your recommendation and changed this parameter. However, this did not solve the problem - there are no signals on the data lines in the command mode.
2023-12-07 8:38 AM
Alex,
Did you ever figure this out? I'm in a very similar situation with an stm32u5a9 driving a ILI9881C. I'm trying to send low power commands to set up the controller but my controller only supports video mode and I'm seeing no signal on the DSI lines.
2025-03-16 9:54 PM
Hi @AlexVetoshko @nwm_35 @wrfrf.1
did you by any chance solve this issue about no command/data on DSI Data Lane 0 in Low Power mode?
Thank you
Rick
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.