Question
STM32F746 ADC DMA buffer overrun when TouchGFX starts
I use a stm32f746 disco board and try to set the adc at a sample rate of 1.8 MPS. The dma transfers starts correct (I toggle a gpio pin in the convert call back to check the samplerate). I start the adc dma before touchGFX is started but as soon touchgfx is started the adc raises a overrun error and the dma transfer stops. I am also not able to restart again. Does any one have experienced such behaviour?
The adc1 dma is configured circular DMA2 stream 4 clock is 108 Mhz div = 4 12 bits 15 cycles gives 1.8 Mbps