cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 with SSD1963 7'' (800x480) Display

himanshusharma
Associate II

Posted on June 20, 2014 at 07:18

Hi, i am working with SSD1963 7''TFT(800x480) with stm32f407 168 MHz discovery board, SSD1963 driver work fine initializing data bus and control pin as GPIO, but with slow response on TFT, right now refresh rate that I am able to achieve is 1 FPS.

As done a lot of search max. 30 FPS can be achieved using FSMC. I took example of darth and update according to my requirement, but some how its not working. Code is attached plz take a look and let me know what I am doing wrong. 

10 REPLIES 10
Posted on September 15, 2014 at 14:43

I m using FMC inside STM32F429ZIT6 to interface the 7 inch touch screen based SSD1963, the lcd is not working correctly. Hence i need some corrections. I m posting my code here.

Stop spamming the forum, open a new topic and post your code ONCE.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..