cancel
Showing results for 
Search instead for 
Did you mean: 

STeMwin GUI_CompactColor_16 problem

liviana
Associate II
Posted on March 10, 2014 at 06:44

Hello! In order to show display in specific LCD like SSD1298, I must configure GUIDRV_CompactColor_16 according tohttp://www.segger.com/guidrv_compactcolor_html. I have made the LCDConfig.c, GUIDRV_CompactColor_c, andGUIDRV_CompactColor_h. But when I tried to debug, it came to hardfault handler, after executing

GUI_DEVICE_CreateAndLink(DISPLAY_DRIVER, COLOR_CONVERSION, 0, 0).

May I ask for explanation? Thank you very much. Here is the code of LCDConfig.c

#include ''GUI.h''
#include ''LCDConf_CompactColor_h''
#include ''GUIDRV_CompactColor_h''
#include ''LCDConf.h''
/*********************************************************************
* Layer configuration
*********************************************************************/
/* Physical display size */
#define XSIZE_PHYS 240 //no change!!
#define YSIZE_PHYS 320 //no change!!
#define VXSIZE_PHYS 240
#define VYSIZE_PHYS 320
/* Color conversion */
#define COLOR_CONVERSION GUICC_M565
/* Display driver */
#define DISPLAY_DRIVER GUIDRV_COMPACT_COLOR_16
//
// Buffers / VScreens
//
#define NUM_BUFFERS 1
#define NUM_VSCREENS 1
//
// Display orientation
//
#define DISPLAY_ORIENTATION 0
//#define DISPLAY_ORIENTATION (GUI_MIRROR_X | GUI_MIRROR_Y)
//#define DISPLAY_ORIENTATION (GUI_SWAP_XY | GUI_MIRROR_X)
//#define DISPLAY_ORIENTATION (GUI_MIRROR_X)
//
// Touch screen
//
#define USE_TOUCH 0
//
// Touch screen calibration
#define TOUCH_X_MIN 0x00E0
#define TOUCH_X_MAX 0x0F40
#define TOUCH_Y_MIN 0x00C0
#define TOUCH_Y_MAX 0x0F60
/*********************************************************************
* Configuration checking
*********************************************************************/
#ifndef VXSIZE_PHYS
#define VXSIZE_PHYS XSIZE_PHYS
#endif
#ifndef VYSIZE_PHYS
#define VYSIZE_PHYS YSIZE_PHYS
#endif
#ifndef XSIZE_PHYS
#error Physical X size of display is not defined!
#endif
#ifndef YSIZE_PHYS
#error Physical Y size of display is not defined!
#endif
#ifndef COLOR_CONVERSION
#error Color conversion not defined!
#endif
#ifndef DISPLAY_DRIVER
#error No display driver defined!
#endif
#ifndef NUM_VSCREENS
#define NUM_VSCREENS 1
#else
#if (NUM_VSCREENS <= 0)
#error At least one screeen needs to be defined!
#endif
#endif
#if (NUM_VSCREENS > 1) && (NUM_BUFFERS > 1)
#error Virtual screens and multiple buffers are not allowed!
#endif
#ifndef LCD_SWAP_XY
#define LCD_SWAP_XY 0
#endif
#if LCD_SWAP_XY
#define LCD_XSIZE YSIZE_PHYS
#define LCD_YSIZE XSIZE_PHYS
#else
#define LCD_XSIZE XSIZE_PHYS
#define LCD_YSIZE YSIZE_PHYS
#endif
#define LCD_VXSIZE LCD_XSIZE
#define LCD_VYSIZE LCD_YSIZE
#ifndef DISPLAY_ORIENTATION
#define DISPLAY_ORIENTATION 0
#endif
#if ((DISPLAY_ORIENTATION & GUI_SWAP_XY) != 0)
#define LANDSCAPE 1
#else
#define LANDSCAPE 0
#endif
#if (LANDSCAPE == 1)
#define WIDTH YSIZE_PHYS /* Screen Width (in pixels) */
#define HEIGHT XSIZE_PHYS /* Screen Hight (in pixels) */
#else
#define WIDTH XSIZE_PHYS /* Screen Width (in pixels) */
#define HEIGHT YSIZE_PHYS /* Screen Hight (in pixels) */
#endif
// #if ((DISPLAY_ORIENTATION & GUI_SWAP_XY) != 0)
// #if ((DISPLAY_ORIENTATION & GUI_MIRROR_X) != 0)
// #define TOUCH_TOP TOUCH_X_MAX
// #define TOUCH_BOTTOM TOUCH_X_MIN
// #else
// #define TOUCH_TOP TOUCH_X_MIN
// #define TOUCH_BOTTOM TOUCH_X_MAX
// #endif
// #if ((DISPLAY_ORIENTATION & GUI_MIRROR_Y) != 0)
// #define TOUCH_LEFT TOUCH_Y_MAX
// #define TOUCH_RIGHT TOUCH_Y_MIN
// #else
// #define TOUCH_LEFT TOUCH_Y_MIN
// #define TOUCH_RIGHT TOUCH_Y_MAX
// #endif
// #else
// #if ((DISPLAY_ORIENTATION & GUI_MIRROR_X) != 0)
// #define TOUCH_LEFT TOUCH_X_MAX
// #define TOUCH_RIGHT TOUCH_X_MIN
// #else
// #define TOUCH_LEFT TOUCH_X_MIN
// #define TOUCH_RIGHT TOUCH_X_MAX
// #endif
// #if ((DISPLAY_ORIENTATION & GUI_MIRROR_Y) != 0)
// #define TOUCH_TOP TOUCH_Y_MAX
// #define TOUCH_BOTTOM TOUCH_Y_MIN
// #else
// #define TOUCH_TOP TOUCH_Y_MIN
// #define TOUCH_BOTTOM TOUCH_Y_MAX
// #endif
// #endif
/*********************************************************************
*
* Access routines
*
*********************************************************************/
/*********************************************************************
*
* Driver Port functions
*
**********************************************************************
*/
extern void LCD_X_Init(void);
extern void LCD_X_Write00_16(U16 c);
extern void LCD_X_Write01_16(U16 c);
extern U16 LCD_X_Read01_16 (void);
extern void LCD_X_WriteM01_16(U16 * pData, int NumWords);
extern void LCD_X_ReadM01_16 (U16 * pData, int NumWords);
static void delay (int cnt) {
cnt <<= 15;
while (cnt--);
}
static void wr_reg (U16 reg, U16 dat) {
LCD_X_Write00_16(reg);
LCD_X_Write01_16(dat);
}
static U16 rd_reg (U16 reg) {
LCD_X_Write00_16(reg);
return LCD_X_Read01_16();
}
/*********************************************************************
*
* LCD_X_InitController
*
* Purpose:
* Initializes the display controller
*/
static void _InitController(void)
{
/* Set up the display controller and put it into operation. If the
* display controller is not initialized by any external routine
* this needs to be adapted by the customer.
*/
static unsigned short driverCode;
LCD_X_Init();
delay(5); /* Delay 50 ms */
driverCode = rd_reg(0x00);
if(driverCode==0x8989)
{
wr_reg(0x0000,0x0001); delay(5);
wr_reg(0x0003,0xA8A4); delay(5);
wr_reg(0x000C,0x0000); delay(5);
wr_reg(0x000D,0x080C); delay(5);
wr_reg(0x000E,0x2B00); delay(5);
wr_reg(0x001E,0x00B0); delay(5);
wr_reg(0x0001,0x2B3F); delay(5);
wr_reg(0x0002,0x0600); delay(5);
wr_reg(0x0010,0x0000); delay(5);
wr_reg(0x0011,0x6070); delay(5); /* Set GRAM write direction */
wr_reg(0x0005,0x0000); delay(5);
wr_reg(0x0006,0x0000); delay(5);
wr_reg(0x0016,0xEF1C); delay(5);
wr_reg(0x0017,0x0003); delay(5);
wr_reg(0x0007,0x0133); delay(5);
wr_reg(0x000B,0x0000); delay(5);
wr_reg(0x000F,0x0000); delay(5);
wr_reg(0x0041,0x0000); delay(5);
wr_reg(0x0042,0x0000); delay(5);
wr_reg(0x0048,0x0000); delay(5);
wr_reg(0x0049,0x013F); delay(5);
wr_reg(0x004A,0x0000); delay(5);
wr_reg(0x004B,0x0000); delay(5);
wr_reg(0x0044,0xEF00); delay(5);
wr_reg(0x0045,0x0000); delay(5);
wr_reg(0x0046,0x013F); delay(5);
wr_reg(0x0030,0x0707); delay(5);
wr_reg(0x0031,0x0204); delay(5);
wr_reg(0x0032,0x0204); delay(5);
wr_reg(0x0033,0x0502); delay(5);
wr_reg(0x0034,0x0507); delay(5);
wr_reg(0x0035,0x0204); delay(5);
wr_reg(0x0036,0x0204); delay(5);
wr_reg(0x0037,0x0502); delay(5);
wr_reg(0x003A,0x0302); delay(5);
wr_reg(0x003B,0x0302); delay(5);
wr_reg(0x0023,0x0000); delay(5);
wr_reg(0x0024,0x0000); delay(5);
wr_reg(0x0025,0x8000); delay(5);
wr_reg(0x004f,0);
wr_reg(0x004e,0);
}
delay(5); /* delay 50 ms */
}
/*********************************************************************
* Public code
*********************************************************************/
/*********************************************************************
*
* LCD_X_Config
*
* Purpose:
* Called during the initialization process in order to set up the
* display driver configuration.
*
*/
void LCD_X_Config(void)
{
//
// Set display driver and color conversion
//
GUI_DEVICE_CreateAndLink(DISPLAY_DRIVER, COLOR_CONVERSION, 0, 0);
//
// Display driver configuration
//
// if (LCD_GetSwapXY()) {
// LCD_SetSizeEx (0, YSIZE_PHYS, XSIZE_PHYS);
// LCD_SetVSizeEx(0, YSIZE_PHYS * NUM_VSCREENS, XSIZE_PHYS);
// } else {
// LCD_SetSizeEx (0, XSIZE_PHYS, YSIZE_PHYS);
// LCD_SetVSizeEx(0, XSIZE_PHYS, YSIZE_PHYS * NUM_VSCREENS);
// }
// #if (USE_TOUCH == 1)
// //
// // Set orientation of touch screen
// //
// GUI_TOUCH_SetOrientation(DISPLAY_ORIENTATION);
// //
// // Calibrate touch screen
// //
// GUI_TOUCH_Calibrate(GUI_COORD_X, 0, WIDTH - 1, TOUCH_LEFT, TOUCH_RIGHT);
// GUI_TOUCH_Calibrate(GUI_COORD_Y, 0, HEIGHT - 1, TOUCH_TOP, TOUCH_BOTTOM);
// #endif
}
/*********************************************************************
*
* LCD_X_DisplayDriver
*
* Purpose:
* This function is called by the display driver for several purposes.
* To support the according task the routine needs to be adapted to
* the display controller. Please note that the commands marked with
* 'optional' are not cogently required and should only be adapted if
* the display controller supports these features.
*
* Parameter:
* LayerIndex - Index of layer to be configured
* Cmd - Please refer to the details in the switch statement below
* pData - Pointer to a LCD_X_DATA structure
*/
int LCD_X_DisplayDriver(unsigned LayerIndex, unsigned Cmd, void * pData) {
int r;
switch (Cmd)
{
/*
* Required
*/
case LCD_X_INITCONTROLLER:
{
/*
* Called during the initialization process in order to set up the
* display controller and put it into operation. If the display
* controller is not initialized by any external routine this needs
* to be adapted by the customer...
*/
_InitController();
r = 0;
break;
}
/* Implement all required tasks for the LCD_X_DisplayDriver function in
* the following section. */
default:
r = -1;
}
return r;
}

Thank you very much for your kindly help. #stemwin #ssd1289
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
joerg23
Associate II
Posted on March 10, 2014 at 20:42

Thats a working config for ssd1289

________________

Attachments :

LCDConf_stm3240g_eval.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzNM&d=%2Fa%2F0X0000000bMR%2FKEuGrg2IwhR27643NJx45ebLiZlTct_WqsnhhjZRRjk&asPdf=false