2022-02-15 7:38 AM
I am currently working on a project that will ultimately involve switching out the native display on the STM32H747I-DISCO with a new one (MDT0500AISC-MIPI). This new display utilizes a MIPI-DSI interface, but unlike the native display, does not have any onboard GRAM. Before switching to the new display, I want to get the native display to run in DSI-video mode in order to prove the STM32H747I-DISCO can drive displays without leveraging on-display GRAM. I have tried to follow every bit of information between datasheets, ST guides, and forum posts that I can, but every attempt has resulted in the display remaining blank.
I am hopeful that someone here has worked through something similar and can help.
Steps I have taken so far:
It is my understanding that I should be able to use CubeMX convert a TouchGFX project from using DSI adapted command mode to using DSI video mode on native hardware without needing to write additional custom code. I think I am close to the proper solution, but I'm obviously missing something.
If anyone has had to go through a similar process and has insight, I would greatly appreciate your input.
2022-02-20 11:53 AM
Maybe at first you dont waste time with LCD if you plan use other.
Every display have own IC controllers and if is different, your code on one dont work on second.
Too your idea with start TGFX isnt simple. Normal way is test display without TGFX first.
Then basic steps for video mode:
/**
* @brief Start test pattern generation
* @param hdsi pointer to a DSI_HandleTypeDef structure that contains
* the configuration information for the DSI.
* @param Mode Pattern generator mode
* This parameter can be one of the following values:
* 0 : Color bars (horizontal or vertical)
* 1 : BER pattern (vertical only)
* @param Orientation Pattern generator orientation
* This parameter can be one of the following values:
* 0 : Vertical color bars
* 1 : Horizontal color bars
* @retval HAL status
*/
HAL_StatusTypeDef HAL_DSI_PatternGeneratorStart(DSI_HandleTypeDef *hdsi, uint32_t Mode, uint32_t Orientation)now try config DSI ... to stable LCD show colour bars, after ok comment out or stop generator and check background color LTDC showed on LCD,
2022-02-21 5:17 AM
Hi,
I’ve had success going through the same process with the STM32F469-DISCO. It did take some persistence!
I would agree with @MM..1 to start without Touchgfx and focus on getting the LCD initialised in video mode and pattern generator working.
It is not a bad option starting with the native LCD on the disco as this eliminates uncertainty about hardware connectivity with your new LCD.
There should be an example project on the ST repo LCD_DSI_VideoMode_SingleBuffer which will include the necessary initialisation commands.