2022-09-12 9:44 AM
I’m trying to run the example of touchgfx stm32g071 nucleo demo, but when I import to stm32ide and debug, the program never returns from the function "void tick" in " HAL::getInstance()->backPorchExited() or do I need to change the code somewhere?
thank you.
2022-09-13 12:09 AM
Hello @BTeof.1 ,
If I understand correctly, you are using TouchGFX 4.16 ?
If yes, could you please upgrade to 4.20 and see if there is still compilation errors ?
Thank you,
/Yoann