cancel
Showing results for 
Search instead for 
Did you mean: 

MIPI DSI_D2 &D3

PAMSA.1
Associate

Hello

I bought an Stm32f769-disco board to evaluate the STM32F7 and I'd mike to go forward on my design...

On the board you have a 4" Mipi Dsi display and I would like to implement a 7" mipi display.

The problem that i found is that most ipi display on the market have 4 serial lines D0 D1 D2 and D3

The LTDC drive on CPU only provide D0 and D1 lines.

How can i make it compatible with other displays??

Thanks for your answer

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0