I do not enter in HSYNC interrupt DCIM STM32H743
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-10-22 6:16 AM
I want to fetch video data from camera via decoder (TVP5150AM1) through DCIM.
I configure decoder to output 4:2:2 8-bit YCbCr video with discrete synchronization and I do not get HSYNC interrupt,
DCMI->IER |= (0x1 << 4) | (0x1 << 0);
so, first time when I enter into the interrupt routine my DMA->NDTR register is already 0x0, what means that I filled up full buffer already, when I expect get HSYNC interrupt after ~760 data transfers.
What do I do wrong?
Labels:
- Labels:
-
DCMI
-
STM32H7 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0