cancel
Showing results for 
Search instead for 
Did you mean: 

HardFault on touchgfx::Application::drawCachedAreas()

I_ve_got_a_problem
Associate III

Hi!

I have a board with a STM32H730 chip, my RAM is configured as not cacheable and instruction access disabled,as performance decreases a lot otherwise, but now i'm getting a hardfault after drawCachedAreas(); is executed,

As i can't see what that function is doing, i thought that mayb someone could help me. 

I_ve_got_a_problem_0-1746167243726.png

 

I_ve_got_a_problem_1-1746167676556.png

I_ve_got_a_problem_3-1746167709207.png

 

 

If someone is invested enough here is my MPU config

void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct; /* 1) Deshabilita el MPU para reconfigurar */ HAL_MPU_Disable(); /* ———————————————————————————————————————————————————— * Región 0: fondo 4 GB NO_ACCESS (cubre todo excepto QSPI, SDRAM y SRAM) *———————————————————————————————————————————————————*/ MPU_InitStruct = (MPU_Region_InitTypeDef){0}; MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0x00000000U; MPU_InitStruct.Size = MPU_REGION_SIZE_4GB; MPU_InitStruct.SubRegionDisable = 0x87; // deja libres subregs 2 y 3 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* ———————————————————————————————————————————————————— * Región 1: QSPI externa @0x9000_0000, 64 MB (XIP) *———————————————————————————————————————————————————*/ MPU_InitStruct = (MPU_Region_InitTypeDef){0}; MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER1; MPU_InitStruct.BaseAddress = 0x90000000U; MPU_InitStruct.Size = MPU_REGION_SIZE_64MB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; // normal, cacheable MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; // XIP MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* ———————————————————————————————————————————————————— * Región 2: SDRAM externa @0x7000_0000, 8 MB <— toda la RAM externa * • non-cacheable (evita incoherencias LTDC/DMA) * • non-bufferable (hace el bus más “estricto” pero es el estado original) * • shareable (mantiene coherencia para masters DMA) *———————————————————————————————————————————————————*/ MPU_InitStruct = (MPU_Region_InitTypeDef){0}; MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER2; MPU_InitStruct.BaseAddress = 0x70000000U; MPU_InitStruct.Size = MPU_REGION_SIZE_8MB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* ———————————————————————————————————————————————————— * Región 3: AXI-SRAM interna @0x2400_0000, 512 KB * • cacheable + bufferable para código/variables críticas *———————————————————————————————————————————————————*/ MPU_InitStruct = (MPU_Region_InitTypeDef){0}; MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER3; MPU_InitStruct.BaseAddress = 0x24000000U; MPU_InitStruct.Size = MPU_REGION_SIZE_512KB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* 2) Reactiva el MPU con “privileged default map” para todo lo que no cubran las regiones anteriores */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); }
View more

Base addresses are all like in the linker file, except flash that starts at 0x90000200


**EDIT** 

I forgot to mention, in the MPU config if i set RAM as cacheable, the hardFault dissapears, but i need it to be not cacheable or i get like 10 times worse performance. 

4 REPLIES 4
GaetanGodart
ST Employee

Hello @I_ve_got_a_problem ,

 

I am no expert on cache but it says it is not aligned.

In the linker script, do you align your sections like we do :

GaetanGodart_0-1746615629663.png

 

Regards,

 

Gaetan Godart
Software engineer at ST (TouchGFX)

Yes!

I also suspected it was an alignment problem, but I have tried different alignments and none have worked, so I came back to the one the .ioc generates for touchgfx, 

What makes it hard to debug, is the fact that I have no clue of what Application::drawCachedAreas() does, since it is already compiled in the touchgfx library.

 

I know the problem isn't the function itself, but rather my MPU_Configuration, but i can't know where is faulting, so I lack a starting point.

 

The problem has been transfered to some colleagues now, and they are trying things, but we could appreciate if you could share some light into what the function does, beyond what the name tells us.

 

Thanks for the response anyways!

GaetanGodart
ST Employee

Hello @I_ve_got_a_problem ,

 

It is quite hard for me to help you on MPU configuration but perhaps I can share some resources that would be useful :

  1. http://st.com/resource/en/application_note/an4838-introduction-to-memory-protection-unit-management-on-stm32-mcus-stmicroelectronics.pdf
  2. https://support.touchgfx.com/docs/development/scenarios/running-graphics-on-stm32h7r

 

Please tell me if it is of any help!

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hello @I_ve_got_a_problem ,

 

Have you been able to move forward on your project?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)