Skip to main content
ferro
Lead
February 20, 2025
Solved

GfxDesigner: drag&drop for project.touchgfx

  • February 20, 2025
  • 6 replies
  • 568 views

Hi Gfx Team,

Could you please implement drag&drop as an alternative to open a project.touchgfx ?

Thank you

    This topic has been closed for replies.
    Best answer by GaetanGodart

    The new incoming version of TouchGFX Designer will open way faster, so if it is just to avoid closing then re-opening TouchGFX Designer because it is slow, it won't be that important soon.

    Perhaps the new incoming version would be a sufficient solution and opening a new project from "File" => "Open" would be a sufficient work around while waiting for the new version?

     

    Regards,

    6 replies

    GaetanGodart
    ST Employee
    February 20, 2025

    Hello @ferro ,

     

    In which case would the drag and drop be useful for you?

    Do you want to be able to drag a .touchgfx project in the Designer main window at any time?
    Do you want to be able to drag a .touchgfx file after clicking on "File" => "Open"?

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    ferro
    ferroAuthor
    Lead
    February 20, 2025

    @GaetanGodart 

    Until now, I've always closed the Designer, clicked on the project.touchgfx and let the OS handle it. Very slow. MSVC IDE spoiled me with my expectations - its very fast.

    I just noticed that keeping the Designer open and opening a project.touchgfx via [file > open] is lightning fast.

    GaetanGodart
    GaetanGodartBest answer
    ST Employee
    February 20, 2025

    The new incoming version of TouchGFX Designer will open way faster, so if it is just to avoid closing then re-opening TouchGFX Designer because it is slow, it won't be that important soon.

    Perhaps the new incoming version would be a sufficient solution and opening a new project from "File" => "Open" would be a sufficient work around while waiting for the new version?

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    ferro
    ferroAuthor
    Lead
    February 20, 2025

    Hi @GaetanGodart 

    "be able to drag a .touchgfx project in the Designer main window at any time?"

    This would be ideal.