cancel
Showing results for 
Search instead for 
Did you mean: 

FrontendHeap store in to external SDRAM hardfault

heyo
Senior

Hi, still can't to upload frontend heap to my 8MB external SDRAM.

My linker script:

 

/*
******************************************************************************
**
**  File        : LinkerScript.ld
**
**  Author      : STM32CubeIDE
**
**  Abstract    : Linker script for STM32H7 series
**                2048Kbytes FLASH and 1056Kbytes RAM
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used.
**
**  Target      : STMicroelectronics STM32
**
**  Distribution: The file is distributed as is, without any warranty
**                of any kind.
**
*****************************************************************************
** @attention
**
** Copyright (c) 2022 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
****************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1);    /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x1000;      /* required amount of heap  */
_Min_Stack_Size = 0x1000; /* required amount of stack */

/* Specify the memory areas */
MEMORY
{
  FLASH (rx)     : ORIGIN = 0x08000000, LENGTH = 2048K
  DTCMRAM (xrw)  : ORIGIN = 0x20000000, LENGTH = 128K
  RAM_D1 (xrw)   : ORIGIN = 0x24000000, LENGTH = 512K
  RAM_D2 (xrw)   : ORIGIN = 0x30000000, LENGTH = 288K
  RAM_D3 (xrw)   : ORIGIN = 0x38000000, LENGTH = 64K
  ITCMRAM (xrw)  : ORIGIN = 0x00000000, LENGTH = 64K
  QUADSPI (r)    : ORIGIN = 0x90000000, LENGTH = 16M
  SDRAM   (xrw)  : ORIGIN = 0xC0000000, LENGTH = 8M
}

/* Define output sections */
SECTIONS
{
  /* The startup code goes first into FLASH */
  .isr_vector :
  {
    . = ALIGN(4);
    KEEP(*(.isr_vector)) /* Startup code */
    . = ALIGN(4);
  } >FLASH
  /* The program code and other data goes into FLASH */
  .text :
  {
    . = ALIGN(4);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)

    KEEP (*(.init))
    KEEP (*(.fini))

    . = ALIGN(4);
    _etext = .;        /* define a global symbols at end of code */
  } >FLASH

  /* Constant data goes into FLASH */
  .rodata :
  {
    . = ALIGN(4);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(4);
  } >FLASH

  .ARM.extab   : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
  .ARM : {
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
  } >FLASH

  .preinit_array     :
  {
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
  } >FLASH

  .init_array :
  {
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
  } >FLASH

  .fini_array :
  {
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
  } >FLASH

  /* used by the startup to initialize data */
  _sidata = LOADADDR(.data);

  /* Initialized data sections goes into RAM, load LMA copy after code */
  .data :
  {
    . = ALIGN(4);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */
    *(.RamFunc)        /* .RamFunc sections */
    *(.RamFunc*)       /* .RamFunc* sections */

    . = ALIGN(4);
    _edata = .;        /* define a global symbol at data end */
  } >RAM_D1 AT> FLASH

  /* Uninitialized data section */
  . = ALIGN(4);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)

    . = ALIGN(4);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >RAM_D1

  /* User_heap_stack section, used to check that there is enough RAM left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >RAM_D1


	.sdram_section (NOLOAD) : { *(.sdram_section) }> SDRAM
  TouchGFX_Framebuffer (NOLOAD) : { *(TouchGFX_Framebuffer) } >SDRAM
  /* Remove information from the standard libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }
  .ARM.attributes 0 : { *(.ARM.attributes) }

      FontFlashSection(NOLOAD) : /*DELETE (NOLOAD) IF U WANT TO UPDATE QSPI FLASH*/
  {
    *(FontFlashSection FontFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >QUADSPI

  TextFlashSection(NOLOAD) :/*DELETE (NOLOAD) IF U WANT TO UPDATE QSPI FLASH*/
  {
    *(TextFlashSection TextFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >QUADSPI

  ExtFlashSection(NOLOAD) :/*DELETE (NOLOAD) IF U WANT TO UPDATE QSPI FLASH*/
  {
    *(ExtFlashSection ExtFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >QUADSPI
}

 

I placed my double framebuffer to other address:

heyo_0-1687933999431.png

Set framebuffer in LTDC start:

heyo_1-1687934027748.png

And add line to FrontendHeap.hpp:

heyo_2-1687934079010.png

And I always get hardfault at : (__attribute__ ((section (".sdram_section")))) .Maybe someone see the mistake and can help? Thank you.

 

This discussion is locked. Please start a new topic to ask your question.
23 REPLIES 23
uilter
Senior

Did you setup your MPU peripheral?

This is an example that works for me, but in my case the SDRAM have 16MB.
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;

 

Do I really need to do that to store frontend heap to my external sdram?

Only if you have enough internal RAM memory, and it will not affect your application, no is not an obligation.

To know it, you need to calculate the size of your frame buffer. "framebuffer is width * height * color depth in bits / 8 bytes." This link is nice to check it https://support.touchgfx.com/docs/basic-concepts/framebuffer#memory-consumption

Another tip, if you are using an external SDRAM, make sure you are able to write and read it.
It may be that your FMC peripheral is wrongly configured, and that is why it is generating these faults.

 

 

My SDRAM working correctly because there I put my framebuffer and it works fine. And when I want to put frontend heap to external SDRAM it crashes at this line : __attribute__ ((section (".sdram_section")))

Sorry, I was thinking you having trouble with framebuffer. Now I understood you want to put the heap in to it.

I never did it. Let wait with anyone can help. I'm curious to know it.

Try to enable MPU, split the SDRAM in regions. I see it in this app note (AN4861), page 87, https://www.st.com/resource/en/application_note/an4861-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf

Likely Hard Faults because you fail to initialize the memory interface before the C/C++ constructors are called.

Should enable the memory in SystemInit(), and in startup.s this should be called before __libc_init_array

Look at the code that's actually faulting to understand why.. the code the MCU is executing at and immediately prior.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

What and where i should enable in this?

 

void SystemInit (void)
{
#if defined (DATA_IN_D2_SRAM)
 __IO uint32_t tmpreg;
#endif /* DATA_IN_D2_SRAM */

  /* FPU settings ------------------------------------------------------------*/
  #if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
    SCB->CPACR |= ((3UL << (10*2))|(3UL << (11*2)));  /* set CP10 and CP11 Full Access */
  #endif
  /* Reset the RCC clock configuration to the default reset state ------------*/
  /* Set HSION bit */
  RCC->CR |= RCC_CR_HSION;

  /* Reset CFGR register */
  RCC->CFGR = 0x00000000;

  /* Reset HSEON, CSSON , CSION,RC48ON, CSIKERON PLL1ON, PLL2ON and PLL3ON bits */
  RCC->CR &= 0xEAF6ED7FU;

#if defined(D3_SRAM_BASE)
  /* Reset D1CFGR register */
  RCC->D1CFGR = 0x00000000;

  /* Reset D2CFGR register */
  RCC->D2CFGR = 0x00000000;

  /* Reset D3CFGR register */
  RCC->D3CFGR = 0x00000000;
#else
  /* Reset CDCFGR1 register */
  RCC->CDCFGR1 = 0x00000000;

  /* Reset CDCFGR2 register */
  RCC->CDCFGR2 = 0x00000000;

  /* Reset SRDCFGR register */
  RCC->SRDCFGR = 0x00000000;
#endif
  /* Reset PLLCKSELR register */
  RCC->PLLCKSELR = 0x00000000;

  /* Reset PLLCFGR register */
  RCC->PLLCFGR = 0x00000000;
  /* Reset PLL1DIVR register */
  RCC->PLL1DIVR = 0x00000000;
  /* Reset PLL1FRACR register */
  RCC->PLL1FRACR = 0x00000000;

  /* Reset PLL2DIVR register */
  RCC->PLL2DIVR = 0x00000000;

  /* Reset PLL2FRACR register */

  RCC->PLL2FRACR = 0x00000000;
  /* Reset PLL3DIVR register */
  RCC->PLL3DIVR = 0x00000000;

  /* Reset PLL3FRACR register */
  RCC->PLL3FRACR = 0x00000000;

  /* Reset HSEBYP bit */
  RCC->CR &= 0xFFFBFFFFU;

  /* Disable all interrupts */
  RCC->CIER = 0x00000000;

#if defined (DATA_IN_D2_SRAM)
  /* in case of initialized data in D2 SRAM (AHB SRAM) , enable the D2 SRAM clock ((AHB SRAM clock) */
#if defined(RCC_AHB2ENR_D2SRAM1EN)
  RCC->AHB2ENR |= (RCC_AHB2ENR_D2SRAM1EN | RCC_AHB2ENR_D2SRAM2EN | RCC_AHB2ENR_D2SRAM3EN);
#else
  RCC->AHB2ENR |= (RCC_AHB2ENR_AHBSRAM1EN | RCC_AHB2ENR_AHBSRAM2EN);
#endif /* RCC_AHB2ENR_D2SRAM1EN */

  tmpreg = RCC->AHB2ENR;
  (void) tmpreg;
#endif /* DATA_IN_D2_SRAM */

#if defined(DUAL_CORE) && defined(CORE_CM4)
  /* Configure the Vector Table location add offset address for cortex-M4 ------------------*/
#ifdef VECT_TAB_SRAM
  SCB->VTOR = D2_AHBSRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
  SCB->VTOR = FLASH_BANK2_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif /* VECT_TAB_SRAM */

#else
  /* dual core CM7 or single core line */
  if((DBGMCU->IDCODE & 0xFFFF0000U) < 0x20000000U)
  {
    /* if stm32h7 revY*/
    /* Change  the switch matrix read issuing capability to 1 for the AXI SRAM target (Target 7) */
    *((__IO uint32_t*)0x51008108) = 0x000000001U;
  }

  /* Configure the Vector Table location add offset address for cortex-M7 ------------------*/
#ifdef VECT_TAB_SRAM
  SCB->VTOR = D1_AXISRAM_BASE  | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal D1 AXI-RAM */
#else
  SCB->VTOR = FLASH_BANK1_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif

#endif /*DUAL_CORE && CORE_CM4*/

}

 

Can I edit startup.s file? It looks like first call __libc_init_array then systeminit.

/* Call the clock system initialization function.*/
  bl  SystemInit

/* Copy the data segment initializers from flash to SRAM */
  ldr r0, =_sdata
  ldr r1, =_edata
  ldr r2, =_sidata
  movs r3, #0
  b LoopCopyDataInit

CopyDataInit:
  ldr r4, [r2, r3]
  str r4, [r0, r3]
  adds r3, r3, #4

LoopCopyDataInit:
  adds r4, r0, r3
  cmp r4, r1
  bcc CopyDataInit
/* Zero fill the bss segment. */
  ldr r2, =_sbss
  ldr r4, =_ebss
  movs r3, #0
  b LoopFillZerobss

FillZerobss:
  str  r3, [r2]
  adds r2, r2, #4

LoopFillZerobss:
  cmp r2, r4
  bcc FillZerobss

/* Call static constructors */
    bl __libc_init_array
/* Call the application's entry point.*/
  bl  main
  bx  lr
.size  Reset_Handler, .-Reset_Handler

 

 

>>What and where i should enable in this?

Clocks, Pins and Peripheral related to the SDRAM

Before it exits, and Before you touch the SDRAM Memory.

startup.s looks to be doing things in an appropriate order. You likely get the Hard Fault currently because you don't initialize the SDRAM properly until you get to main()

https://github.com/STMicroelectronics/STM32CubeH7/blob/master/Projects/STM32H747I-EVAL/Applications/USB_Device/CustomHID_Standalone/Common/Src/system_stm32h7xx.c#L384

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

But framebuffer in external SDRAM is placed perfectly and working fine until I write this line : __attribute__ ((section (".sdram_section"))) before : static FrontendHeap instance;