2015-12-03 9:51 PM
Hi All!
Today I found the strange mistake(?)
In the file of demo application for
STM32f429I- DiscoveryLCDConf_stm32f429i_disco_MB1c string 328 we can see function
HAL_LTDC_LineEvenCallback(LTDC_HandleTypeDef *hltdc) . How I understund This function NEVER call.
I think this function must be call in ISR of LTDC. But the name is mistake(?) In the name of this function is ''Even'' NOT ''Event''. It is right??
My be this mistake and
/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/STemWin%20in%20landscape%20with%20Cube%20%2b%20STM32F429discovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=1153
link together??Now I can not check it....
#stm2015-12-04 5:07 AM
Hi kosenko.pavel,
''But the name is mistake(?) In the name of this function is ''Even'' NOT ''Event''. It is right??'' In fact,this bug is fixed by creating an aliased function in the stm32_hal_legacy.h file: #define HAL_LTDC_LineEvenCallback HAL_LTDC_LineEventCallback for the display orientation issue check Heisenburg response in this -Syrine-2015-12-04 6:06 AM
The display orientation on Disco doesn't work correct. When display rotate I see artifacts on display.
Now I try to adapted the SEGGER driver to Disco and the first experiment show good results. No artifacts! But in this case I have ''hell mixed'' SPL and HAL ;) I hope to make all in one style but now it is mixed. I like style from ST and hope that this bug will be find.